TableSectionBuilder Class¶
-
class
NXOpen.Annotations.
TableSectionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.TableSection
builderTo create a new instance of this class, use
NXOpen.Annotations.TableSectionCollection.CreateTableSectionBuilder()
Default values.
Property Value ColumnWidth 50 (millimeters part), 2 (inches part) NumberOfColumns 5 NumberOfRows 5 RowHeight 8 (millimeters part), 0.25 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ColumnWidth | Returns or sets the column width |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for the annotation |
NumberOfColumns | Returns or sets the number of columns, input for tabulr note column numbers |
NumberOfRows | Returns or sets the number of rows |
Origin | Returns the origin, where the symbol is going to be displayed |
RowHeight | Returns or sets the row height |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ColumnWidth¶
-
TableSectionBuilder.
ColumnWidth
¶ Returns or sets the column width
-------------------------------------
Getter Method
Signature
ColumnWidth()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColumnWidth(columnWidth)
Parameters: columnWidth (float) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Leader¶
-
TableSectionBuilder.
Leader
¶ Returns the
NXOpen.Annotations.LeaderBuilder
for the annotation-------------------------------------
Getter Method
Signature
Leader()
Returns: Return type: NXOpen.Annotations.LeaderBuilder
New in version NX8.0.0.
License requirements: None.
NumberOfColumns¶
-
TableSectionBuilder.
NumberOfColumns
¶ Returns or sets the number of columns, input for tabulr note column numbers
-------------------------------------
Getter Method
Signature
NumberOfColumns()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfColumns(numberOfColumns)
Parameters: numberOfColumns (int) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
NumberOfRows¶
-
TableSectionBuilder.
NumberOfRows
¶ Returns or sets the number of rows
-------------------------------------
Getter Method
Signature
NumberOfRows()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfRows(numberOfRows)
Parameters: numberOfRows (int) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Origin¶
-
TableSectionBuilder.
Origin
¶ Returns the origin, where the symbol is going to be displayed
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX8.0.0.
License requirements: None.
RowHeight¶
-
TableSectionBuilder.
RowHeight
¶ Returns or sets the row height
-------------------------------------
Getter Method
Signature
RowHeight()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RowHeight(rowHeight)
Parameters: rowHeight (float) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Style¶
-
TableSectionBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.TableStyleBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TableSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.