TableCellStyleBuilderFormatType Enumeration

NXOpen.Annotations.TableCellStyleBuilder.FormatType is an alias for NXOpen.Annotations.TableCellStyleBuilderFormatType

class NXOpen.Annotations.TableCellStyleBuilderFormatType

Bases: object

the valid cell format types

Deprecated since version NX10.0.0: Use NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes instead.

Enum Members

Enum Member Enum Member Description
Text
Float
Fixed
General
Monetary
Comma
FractionHalfSize
FractionThreeQuarterSize
FractionFullSize
DegreesDegreeUnits
Degrees
DegreesRadianUnits
Radians
Percent
Degrees
Radians
Hex
Logic
DateDmy
DateDm
DateMy
DateMdy
DateYmd
DateY4md
DateDmyDot
TimeHm
TimeHms
Hidden
Custom
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.