TableCellStyleBuilderCellFormatTypes Enumeration

NXOpen.Annotations.TableCellStyleBuilder.CellFormatTypes is an alias for NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes

class NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes

Bases: object

the cell format types

Enum Members

Enum Member Enum Member Description
Text
Text
Float
Float
Fixed
Fixed
General
General
Monetary
Monetary
Comma
Comma
FractionHalfSize
Fraction half size
FractionThreeQuarterSize
Fraction three quarter size
FractionFullSize
Fraction full size
DegreesDegreeUnits
Degrees
DegreesRadianUnits
Radians
Percent
Percent
Degrees
Radians
Hex
Hex
Logic
Logic
Hidden
Hidden
Custom
Custom
Date
Date
Time
Time
DateTime
Date-Time
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.