SpecificNoteBuilder Class¶
-
class
NXOpen.Annotations.
SpecificNoteBuilder
¶ Bases:
NXOpen.Annotations.PmiAttributeBuilder
Represents a
NXOpen.Annotations.SpecificNote
builderTo create a new instance of this class, use
NXOpen.Annotations.PmiAttributeCollection.CreateSpecificNoteBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AssociatedObjects | Returns the NXOpen.Annotations.AssociatedObjectsBuilder for the annotation |
Attribute | Returns or sets the NXOpen.Annotations.Pmi for this annotation |
BusinessModifier | Returns or sets the business modifier |
Category | Returns or sets the category |
Identifier | Returns or sets the identifier |
KnowledgeFusionClassName | Returns or sets the knowledge fusion class name file, the default class is UG provided pmi KF class |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for the annotation |
Origin | Returns the NXOpen.Annotations.OriginBuilder for the annotation |
Revision | Returns or sets the revision |
Style | Returns the NXOpen.Annotations.StyleBuilder for the annotation |
Tag | Returns the Tag for this object. |
Title | Returns or sets the str title |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributeValues | Returns the attribute values @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetText | Returns the text @return |
SetAttributeValues | Sets the attribute values |
SetText | Sets the text |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Category¶
-
SpecificNoteBuilder.
Category
¶ Returns or sets the category
-------------------------------------
Getter Method
Signature
Category()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Category(category)
Parameters: category (str) – New in version NX6.0.0.
License requirements: None.
Identifier¶
-
SpecificNoteBuilder.
Identifier
¶ Returns or sets the identifier
-------------------------------------
Getter Method
Signature
Identifier()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Identifier(identifier)
Parameters: identifier (str) – New in version NX6.0.0.
License requirements: None.
Revision¶
-
SpecificNoteBuilder.
Revision
¶ Returns or sets the revision
-------------------------------------
Getter Method
Signature
Revision()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Revision(revision)
Parameters: revision (str) – New in version NX6.0.0.
License requirements: None.
Title¶
-
SpecificNoteBuilder.
Title
¶ Returns or sets the str title
-------------------------------------
Getter Method
Signature
Title()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Title(title)
Parameters: title (str) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetText¶
-
SpecificNoteBuilder.
GetText
¶ Returns the text
Signature
GetText()
Returns: Return type: list of str New in version NX6.0.0.
License requirements: None.
SetText¶
-
SpecificNoteBuilder.
SetText
¶ Sets the text
Signature
SetText(text)
Parameters: text (list of str) – New in version NX6.0.0.
License requirements: None.
Validate¶
-
SpecificNoteBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.