RectangularTargetData Class

class NXOpen.Annotations.RectangularTargetData

Bases: NXOpen.Annotations.DatumTargetData

Represents rectangular datum target data

New in version NX4.0.0.

Properties

Property Description
DatumLabel Returns or sets the datum label.
Index Returns or sets the target index.

Methods

Method Description
Dispose Frees the object from memory.
GetLength Returns the length @return Length data
GetSimpleDraftingAidPreferences Returns the SimpleDraftingAidPreferences object @return Datum target preferences
GetWidth Returns the width @return Width data
SetLength Sets the length.
SetSimpleDraftingAidPreferences Sets the SimpleDraftingAidPreferences object
SetWidth Sets the width.

Method Detail

Dispose

RectangularTargetData.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX4.0.0.

License requirements: None.

GetLength

RectangularTargetData.GetLength

Returns the length

Signature GetLength()

Returns:Length data
Return type:NXOpen.Annotations.Value

New in version NX4.0.0.

License requirements: None.

GetWidth

RectangularTargetData.GetWidth

Returns the width

Signature GetWidth()

Returns:Width data
Return type:NXOpen.Annotations.Value

New in version NX4.0.0.

License requirements: None.

SetLength

RectangularTargetData.SetLength

Sets the length.

NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.

Signature SetLength(length)

Parameters:length (NXOpen.Annotations.Value) – New length data

New in version NX4.0.0.

License requirements: None.

SetWidth

RectangularTargetData.SetWidth

Sets the width.

NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.

Signature SetWidth(width)

Parameters:width (NXOpen.Annotations.Value) – New width data

New in version NX4.0.0.

License requirements: None.