DatumTargetData Class

class NXOpen.Annotations.DatumTargetData

Bases: NXOpen.TransientObject

Represents datum target data

New in version NX4.0.0.

Properties

Property Description
DatumLabel Returns or sets the datum label.
Index Returns or sets the target index.

Methods

Method Description
Dispose Frees the object from memory.
GetSimpleDraftingAidPreferences Returns the SimpleDraftingAidPreferences object @return Datum target preferences
SetSimpleDraftingAidPreferences Sets the SimpleDraftingAidPreferences object

Property Detail

DatumLabel

DatumTargetData.DatumLabel

Returns or sets the datum label.

NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.

-------------------------------------

Getter Method

Signature DatumLabel()

Returns:Datum label
Return type:str

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumLabel(datumLabel)

Parameters:datumLabel (str) – New datum label

New in version NX4.0.0.

License requirements: None.

Index

DatumTargetData.Index

Returns or sets the target index.

NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.

-------------------------------------

Getter Method

Signature Index()

Returns:Target index
Return type:int

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Index(index)

Parameters:index (int) – New target index

New in version NX4.0.0.

License requirements: None.

Method Detail

Dispose

DatumTargetData.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX4.0.0.

License requirements: None.

GetSimpleDraftingAidPreferences

DatumTargetData.GetSimpleDraftingAidPreferences

Returns the SimpleDraftingAidPreferences object

Signature GetSimpleDraftingAidPreferences()

Returns:Datum target preferences
Return type:NXOpen.Annotations.SimpleDraftingAidPreferences

New in version NX4.0.0.

License requirements: None.

SetSimpleDraftingAidPreferences

DatumTargetData.SetSimpleDraftingAidPreferences

Sets the SimpleDraftingAidPreferences object

Signature SetSimpleDraftingAidPreferences(preferences)

Parameters:preferences (NXOpen.Annotations.SimpleDraftingAidPreferences) – New datum target preferences

New in version NX4.0.0.

License requirements: None.