RadialDimensionBuilder Class¶
-
class
NXOpen.Annotations.
RadialDimensionBuilder
¶ Bases:
NXOpen.Annotations.BaseRadialDimensionBuilder
Represents a
Annotations.Dimension
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreateRadialDimensionBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AppendedText | Returns the appended text |
DiameterDimensionDimLineAngle | Returns or sets the diameter dimension’s dimension-line-angle |
Driving | Returns the driving |
FirstAssociativity | Returns the first associativity. |
FoldLocation | Returns the fold location |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
Inherit | Returns the inherit |
IsAutoplaced | Returns or sets a flag to indicate if auto placement turned on. |
IsFoldedRadius | Returns or sets the is folded radius |
IsHoleStyle | Returns or sets the is hole style dimension |
IsRadiusToCenter | Returns or sets the is radius to center |
Measurement | Returns the measurement |
OffsetCenterPoint | Returns the offset center point |
Origin | Returns the origin |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNthSecondaryArrowheadOrientation | The arrowhead orientation for nth secondary dimensions @return |
GetNthSecondaryOrigin | The origins for secondary dimensions @return |
GetObject | Returns the object currently being edited by this builder. |
GetSecondaryCallouts | The secondary callouts @return |
SetNthSecondaryArrowheadOrientation | The arrowhead orientation for nth secondary dimensions |
SetNthSecondaryOrigin | The origins for secondary dimensions |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Driving¶
-
RadialDimensionBuilder.
Driving
¶ Returns the driving
-------------------------------------
Getter Method
Signature
Driving()
Returns: Return type: NXOpen.Annotations.DrivingValueBuilder
New in version NX9.0.0.
License requirements: None.
ForeshorteningSymbol¶
-
RadialDimensionBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
IsAutoplaced¶
-
RadialDimensionBuilder.
IsAutoplaced
¶ Returns or sets a flag to indicate if auto placement turned on.
This is used to compute origins for secondary dimensions
-------------------------------------
Getter Method
Signature
IsAutoplaced()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAutoplaced(isAutoplaced)
Parameters: isAutoplaced (bool) – New in version NX11.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
GetNthSecondaryArrowheadOrientation¶
-
RadialDimensionBuilder.
GetNthSecondaryArrowheadOrientation
¶ The arrowhead orientation for nth secondary dimensions
Signature
GetNthSecondaryArrowheadOrientation(nth)
Parameters: nth (int) – Returns: Return type: NXOpen.Annotations.TextPlacement
New in version NX11.0.0.
License requirements: None.
GetNthSecondaryOrigin¶
-
RadialDimensionBuilder.
GetNthSecondaryOrigin
¶ The origins for secondary dimensions
Signature
GetNthSecondaryOrigin(nth)
Parameters: nth (int) – Returns: Return type: NXOpen.Point3d
New in version NX11.0.0.
License requirements: None.
GetSecondaryCallouts¶
-
RadialDimensionBuilder.
GetSecondaryCallouts
¶ The secondary callouts
Signature
GetSecondaryCallouts()
Returns: Return type: list of NXOpen.Annotations.Dimension
New in version NX11.0.0.
License requirements: None.
SetNthSecondaryArrowheadOrientation¶
-
RadialDimensionBuilder.
SetNthSecondaryArrowheadOrientation
¶ The arrowhead orientation for nth secondary dimensions
Signature
SetNthSecondaryArrowheadOrientation(nth, secondaryArrowheadOrientation)
Parameters: - nth (int) –
- secondaryArrowheadOrientation (
NXOpen.Annotations.TextPlacement
) –
New in version NX11.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetNthSecondaryOrigin¶
-
RadialDimensionBuilder.
SetNthSecondaryOrigin
¶ The origins for secondary dimensions
Signature
SetNthSecondaryOrigin(nth, secondaryOrigin)
Parameters: - nth (int) –
- secondaryOrigin (
NXOpen.Point3d
) –
New in version NX11.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Validate¶
-
RadialDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.