PmiAngularDimensionBuilder Class

class NXOpen.Annotations.PmiAngularDimensionBuilder

Bases: NXOpen.Annotations.BaseAngularDimensionBuilder

Represents a Annotations.AngularDimension builder

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
AppendedText Returns the appended text
AssociatedObjects Returns the associated objects
FirstAssociativity Returns the first associativity
FirstVector Returns or sets the first vector
FirstVectorView Returns or sets the first vector view
Inherit Returns the inherit
Origin Returns the origin
SecondAssociativity Returns the second associativity
SecondVector Returns or sets the second vector
SecondVectorView Returns or sets the second vector view
Style Returns the style
Tag Returns the Tag for this object.

Methods

Method Description
AlternateAngle Alternate angle
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFirstAssociativityVectorFlipped First associativity vector flipped @return
GetObject Returns the object currently being edited by this builder.
GetSecondAssociativityVectorFlipped Second associativity vector flipped @return
SetFirstAssociativityVectorFlipped First associativity vector flipped
SetSecondAssociativityVectorFlipped Second associativity vector flipped
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AssociatedObjects

PmiAngularDimensionBuilder.AssociatedObjects

Returns the associated objects

-------------------------------------

Getter Method

Signature AssociatedObjects()

Returns:
Return type:NXOpen.Annotations.AssociatedObjectsBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

PmiAngularDimensionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.