PartSymbolFolderCollection Class¶
-
class
NXOpen.Annotations.
PartSymbolFolderCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.PartSymbolFolder
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreatePartSymbolFolderBuilder | Creates part symbol folder builder instance @return |
FindObject | Finds the NXOpen.Annotations.PartSymbolFolder with the given name. |
Method Detail¶
CreatePartSymbolFolderBuilder¶
-
PartSymbolFolderCollection.
CreatePartSymbolFolderBuilder
¶ Creates part symbol folder builder instance
Signature
CreatePartSymbolFolderBuilder(currentFolder)
Parameters: currentFolder ( NXOpen.Annotations.PartSymbolFolder
) –NXOpen.Annotations.PartSymbolFolder
to be set as current folderReturns: Return type: NXOpen.Annotations.PartSymbolFolderBuilder
New in version NX6.0.0.
License requirements: None.
FindObject¶
-
PartSymbolFolderCollection.
FindObject
¶ Finds the
NXOpen.Annotations.PartSymbolFolder
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Part symbol folder name Returns: Part symbol folder object Return type: NXOpen.Annotations.PartSymbolFolder
New in version NX7.5.0.
License requirements: None.