PartSymbolFolderBuilder Class¶
-
class
NXOpen.Annotations.
PartSymbolFolderBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.PartSymbolFolderBuilder
.To create a new instance of this class, use
NXOpen.Annotations.PartSymbolFolderCollection.CreatePartSymbolFolderBuilder()
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetChildren | Returns children of current folder @return array of sub folders |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCurrentFolder | Returns current folder @return current folder |
GetFolderCount | Returns number of child folders of current folder @return number of child folders |
GetFolderName | Returns the folder name @return folder name |
GetObject | Returns the object currently being edited by this builder. |
GetParent | Returns parent of current folder provided current folder is not root folder @return parent part symbol folder |
GetPartSymbolCount | Returns number of part symbols of current folder @return number of part symbols |
GetPartSymbols | Returns part symbols of current folder @return array of part symbols |
GetRootFolder | Get the root part symbol folder @return root part symbol folder |
IsRootFolder | Checks whether the given folder is root folder or not @return returns true if root folder |
SetFolderName | Sets folder name provided current folder is not root folder |
SetParent | Sets parent of current folder provided current folder is not root folder |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetChildren¶
-
PartSymbolFolderBuilder.
GetChildren
¶ Returns children of current folder
Signature
GetChildren()
Returns: array of sub folders Return type: list of NXOpen.Annotations.PartSymbolFolder
New in version NX7.5.0.
License requirements: None.
GetCurrentFolder¶
-
PartSymbolFolderBuilder.
GetCurrentFolder
¶ Returns current folder
Signature
GetCurrentFolder()
Returns: current folder Return type: NXOpen.Annotations.PartSymbolFolder
New in version NX7.5.0.
License requirements: None.
GetFolderCount¶
-
PartSymbolFolderBuilder.
GetFolderCount
¶ Returns number of child folders of current folder
Signature
GetFolderCount()
Returns: number of child folders Return type: int New in version NX7.5.0.
License requirements: None.
GetFolderName¶
-
PartSymbolFolderBuilder.
GetFolderName
¶ Returns the folder name
Signature
GetFolderName()
Returns: folder name Return type: str New in version NX7.5.0.
License requirements: None.
GetParent¶
-
PartSymbolFolderBuilder.
GetParent
¶ Returns parent of current folder provided current folder is not root folder
Signature
GetParent()
Returns: parent part symbol folder Return type: NXOpen.Annotations.PartSymbolFolder
New in version NX7.5.0.
License requirements: None.
GetPartSymbolCount¶
-
PartSymbolFolderBuilder.
GetPartSymbolCount
¶ Returns number of part symbols of current folder
Signature
GetPartSymbolCount()
Returns: number of part symbols Return type: int New in version NX7.5.0.
License requirements: None.
GetPartSymbols¶
-
PartSymbolFolderBuilder.
GetPartSymbols
¶ Returns part symbols of current folder
Signature
GetPartSymbols()
Returns: array of part symbols Return type: list of NXOpen.Annotations.MasterSymbol
New in version NX7.5.0.
License requirements: None.
GetRootFolder¶
-
PartSymbolFolderBuilder.
GetRootFolder
¶ Get the root part symbol folder
Signature
GetRootFolder()
Returns: root part symbol folder Return type: NXOpen.Annotations.PartSymbolFolder
New in version NX7.5.0.
License requirements: None.
IsRootFolder¶
-
PartSymbolFolderBuilder.
IsRootFolder
¶ Checks whether the given folder is root folder or not
Signature
IsRootFolder()
Returns: returns true if root folder Return type: bool New in version NX7.5.0.
License requirements: None.
SetFolderName¶
-
PartSymbolFolderBuilder.
SetFolderName
¶ Sets folder name provided current folder is not root folder
Signature
SetFolderName(folderName)
Parameters: folderName (str) – folder name New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
SetParent¶
-
PartSymbolFolderBuilder.
SetParent
¶ Sets parent of current folder provided current folder is not root folder
Signature
SetParent(parentfolder)
Parameters: parentfolder ( NXOpen.Annotations.PartSymbolFolder
) – parent part symbol folderNew in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
PartSymbolFolderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.