MasterCustomSymbolData Class

class NXOpen.Annotations.MasterCustomSymbolData

Bases: NXOpen.TransientObject

Represents master custom symbol data

New in version NX6.0.0.

Deprecated since version NX9.0.0: Use NXOpen.Annotations.MasterSymbolBuilder instead.

Properties

Property Description
Anchor Returns or sets the anchor point
PartName Returns or sets the master part name
SymbolName Returns or sets the symbol name

Methods

Method Description
Dispose Frees the object from memory.
GetPath Get the path for part name @return Path
SetGeometry Specify the geometry for this master custom symbol data.
SetPath Set the valid path for part name

Property Detail

Anchor

MasterCustomSymbolData.Anchor

Returns or sets the anchor point

-------------------------------------

Getter Method

Signature Anchor()

Returns:Anchor point
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Anchor(anchor)

Parameters:anchor (NXOpen.Point) – New anchor point

New in version NX6.0.0.

License requirements: None.

PartName

MasterCustomSymbolData.PartName

Returns or sets the master part name

-------------------------------------

Getter Method

Signature PartName()

Returns:The master part name
Return type:str

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PartName(name)

Parameters:name (str) – New master part name

New in version NX6.0.0.

License requirements: None.

SymbolName

MasterCustomSymbolData.SymbolName

Returns or sets the symbol name

-------------------------------------

Getter Method

Signature SymbolName()

Returns:Symbol name
Return type:str

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymbolName(name)

Parameters:name (str) – New symbol name

New in version NX6.0.0.

License requirements: None.

Method Detail

Dispose

MasterCustomSymbolData.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetPath

MasterCustomSymbolData.GetPath

Get the path for part name

Signature GetPath()

Returns:Path
Return type:str

New in version NX7.5.2.

License requirements: None.

SetGeometry

MasterCustomSymbolData.SetGeometry

Specify the geometry for this master custom symbol data.

Signature SetGeometry(geom)

Parameters:geom (list of NXOpen.DisplayableObject) – symbol geometry

New in version NX6.0.0.

License requirements: None.

SetPath

MasterCustomSymbolData.SetPath

Set the valid path for part name

Signature SetPath(path)

Parameters:path (str) – New path

New in version NX7.5.2.

License requirements: None.