ImportAutocadBlockBuilder Class¶
-
class
NXOpen.Annotations.
ImportAutocadBlockBuilder
¶ Bases:
NXOpen.Builder
Represents a builder allowing import of AutoCAD blocks.
To create a new instance of this class, use
NXOpen.DraftingManager.CreateImportAutocadBlockBuilder()
Default values.
Property Value IncludeSubfolders 0 PreserveFolderStructure 0 SelectMode File New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ImportEntityType | Returns or sets the Import Entity type. |
ImportPolylineTo | Returns or sets the Import polyline option |
IncludeModelSpace | Returns or sets the model space toggle |
IncludeSubfolders | Returns or sets the subfolders toggle |
InputFolder | Returns or sets the name of the input folder |
LibraryPathName | Returns or sets the Reuse library path name. |
PreserveFolderStructure | Returns or sets the folder structure toggle |
SelectMode | Returns or sets the selection mode |
SettingsFile | Returns or sets the AutoCAD setting file |
SymbolType | Returns or sets the Symbol type. |
Tag | Returns the Tag for this object. |
Unit | Returns or sets the symbol part unit |
Methods¶
Method | Description |
---|---|
AddFile | Adds a file to import list |
AddFolder | Adds a folder to import list |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveFile | Removes a file from import list |
RemoveFolder | Removes a folder from import list |
SelectBlock | Selects or deselects a block. |
SelectFile | Selects or deselects a file |
SelectFolder | Selects or deselects a folder |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ImportAutocadBlockBuilderEntityType Enumeration | Represents the Import Entity Type. |
ImportAutocadBlockBuilderFileFolder Enumeration | the Selection mode Enum |
ImportAutocadBlockBuilderType Enumeration | Symbol Type Enum. |
Property Detail¶
ImportEntityType¶
-
ImportAutocadBlockBuilder.
ImportEntityType
¶ Returns or sets the Import Entity type.
-------------------------------------
Getter Method
Signature
ImportEntityType()
Returns: Return type: NXOpen.Annotations.ImportAutocadBlockBuilderEntityType
New in version NX11.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
ImportEntityType(entityType)
Parameters: entityType ( NXOpen.Annotations.ImportAutocadBlockBuilderEntityType
) –New in version NX11.0.0.
License requirements: nx_layout (“NX Layout”)
ImportPolylineTo¶
-
ImportAutocadBlockBuilder.
ImportPolylineTo
¶ Returns or sets the Import polyline option
-------------------------------------
Getter Method
Signature
ImportPolylineTo()
Returns: Return type: int New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
ImportPolylineTo(type)
Parameters: type (int) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
IncludeModelSpace¶
-
ImportAutocadBlockBuilder.
IncludeModelSpace
¶ Returns or sets the model space toggle
-------------------------------------
Getter Method
Signature
IncludeModelSpace()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
IncludeModelSpace(includeModelSpace)
Parameters: includeModelSpace (bool) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
IncludeSubfolders¶
-
ImportAutocadBlockBuilder.
IncludeSubfolders
¶ Returns or sets the subfolders toggle
-------------------------------------
Getter Method
Signature
IncludeSubfolders()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
IncludeSubfolders(includeSubfolders)
Parameters: includeSubfolders (bool) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
InputFolder¶
-
ImportAutocadBlockBuilder.
InputFolder
¶ Returns or sets the name of the input folder
-------------------------------------
Getter Method
Signature
InputFolder()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
InputFolder(foldername)
Parameters: foldername (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
LibraryPathName¶
-
ImportAutocadBlockBuilder.
LibraryPathName
¶ Returns or sets the Reuse library path name.
-------------------------------------
Getter Method
Signature
LibraryPathName()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
LibraryPathName(pathName)
Parameters: pathName (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
PreserveFolderStructure¶
-
ImportAutocadBlockBuilder.
PreserveFolderStructure
¶ Returns or sets the folder structure toggle
-------------------------------------
Getter Method
Signature
PreserveFolderStructure()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
PreserveFolderStructure(preserveFolderStructure)
Parameters: preserveFolderStructure (bool) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SelectMode¶
-
ImportAutocadBlockBuilder.
SelectMode
¶ Returns or sets the selection mode
-------------------------------------
Getter Method
Signature
SelectMode()
Returns: Return type: NXOpen.Annotations.ImportAutocadBlockBuilderFileFolder
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
SelectMode(selectMode)
Parameters: selectMode ( NXOpen.Annotations.ImportAutocadBlockBuilderFileFolder
) –New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SettingsFile¶
-
ImportAutocadBlockBuilder.
SettingsFile
¶ Returns or sets the AutoCAD setting file
-------------------------------------
Getter Method
Signature
SettingsFile()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
SettingsFile(settingsFile)
Parameters: settingsFile (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SymbolType¶
-
ImportAutocadBlockBuilder.
SymbolType
¶ Returns or sets the Symbol type.
Used to differentiate native, teamcenter and part folder modes
-------------------------------------
Getter Method
Signature
SymbolType()
Returns: Return type: NXOpen.Annotations.ImportAutocadBlockBuilderType
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
SymbolType(symbolType)
Parameters: symbolType ( NXOpen.Annotations.ImportAutocadBlockBuilderType
) –New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
Unit¶
-
ImportAutocadBlockBuilder.
Unit
¶ Returns or sets the symbol part unit
-------------------------------------
Getter Method
Signature
Unit()
Returns: Return type: int New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
Unit(unit)
Parameters: unit (int) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
Method Detail¶
AddFile¶
-
ImportAutocadBlockBuilder.
AddFile
¶ Adds a file to import list
Signature
AddFile(fileName)
Parameters: fileName (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
AddFolder¶
-
ImportAutocadBlockBuilder.
AddFolder
¶ Adds a folder to import list
Signature
AddFolder(folderName)
Parameters: folderName (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
RemoveFile¶
-
ImportAutocadBlockBuilder.
RemoveFile
¶ Removes a file from import list
Signature
RemoveFile(fileName)
Parameters: fileName (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
RemoveFolder¶
-
ImportAutocadBlockBuilder.
RemoveFolder
¶ Removes a folder from import list
Signature
RemoveFolder(folderName)
Parameters: folderName (str) – New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SelectBlock¶
-
ImportAutocadBlockBuilder.
SelectBlock
¶ Selects or deselects a block.
Both file and block names need to be specified
Signature
SelectBlock(fileName, blockName, isSelected)
Parameters: - fileName (str) –
- blockName (str) –
- isSelected (bool) –
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SelectFile¶
-
ImportAutocadBlockBuilder.
SelectFile
¶ Selects or deselects a file
Signature
SelectFile(fileName, isSelected)
Parameters: - fileName (str) –
- isSelected (bool) –
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
SelectFolder¶
-
ImportAutocadBlockBuilder.
SelectFolder
¶ Selects or deselects a folder
Signature
SelectFolder(folderName, isSelected)
Parameters: - folderName (str) –
- isSelected (bool) –
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
Validate¶
-
ImportAutocadBlockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.