ImportAutocadBlockBuilderType Enumeration

NXOpen.Annotations.ImportAutocadBlockBuilder.Type is an alias for NXOpen.Annotations.ImportAutocadBlockBuilderType

class NXOpen.Annotations.ImportAutocadBlockBuilderType

Bases: object

Symbol Type Enum.

This option is used to differentiate OS, Teamcenter and Part symbols

Enum Members

Enum Member Enum Member Description
Teamcenter
Teamcenter Symbol
Part
Part Symbol
Native
OS Symbol
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.