DraftingDatumTargetBuilder Class¶
-
class
NXOpen.Annotations.
DraftingDatumTargetBuilder
¶ Bases:
NXOpen.Annotations.DatumTargetBuilder
Represents a
NXOpen.Annotations.DraftingDatumTargetBuilder
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateDraftingDatumTargetBuilder()
Default values.
Property Value Height.Value 10 (millimeters part), 1 (inches part) InnerDiameter.Value 10 (millimeters part), .1 (inches part) OuterDiameter.Value 10 (millimeters part), 1 (inches part) Width.Value 10 (millimeters part), 1 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AreaSize | Returns or sets the area size |
DatumTargetStandard | Returns or sets the datum target standard. |
DrawX | Returns or sets the draw x |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
Height | Returns the height |
Index | Returns or sets the index |
InnerDiameter | Returns the inner diameter |
Label | Returns or sets the label |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for the annotation |
Movable | Returns or sets the flag that indicates movable . |
MovableModifierAngle | Returns the movable modifier angle |
Origin | Returns the origin |
OuterDiameter | Returns the outer diameter |
Style | Returns the style |
Tag | Returns the Tag for this object. |
TerminatorType | Returns or sets the terminator type |
Type | Returns or sets the type |
Width | Returns the width |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InheritFrom | The datum target is inherited form existing datum target. |
ReverseMovableModifier | Reverses the Movable datum target direction by 180 degree |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ForeshorteningSymbol¶
-
DraftingDatumTargetBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DraftingDatumTargetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.