CustomSymbolData Class

class NXOpen.Annotations.CustomSymbolData

Bases: NXOpen.TransientObject

Represents custom symbol data

New in version NX4.0.0.

Deprecated since version NX9.0.0: Use Annotations.DraftingCustomSymbolBuilder for Drafting Custom Symbol and Annotations.PmiCustomSymbolBuilder for PMI Custom Symbol objects.

Properties

Property Description
Angle Returns or sets the angle
Scale Returns or sets the scale
ScaleExpression Returns or sets the scale expression
SymbolPreferencesOption Returns or sets the symbol preferences option.
TextPreferencesOption Returns or sets the text preferences option.

Methods

Method Description
Dispose Frees the object from memory.
GetTextData Return the text data @return List of text data objects
SetTextData Sets the text data

Property Detail

Angle

CustomSymbolData.Angle

Returns or sets the angle

-------------------------------------

Getter Method

Signature Angle()

Returns:Angle at which custom symbol is oriented
Return type:float

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Angle(angle)

Parameters:angle (float) – New angle at which custom symbol will be oriented

New in version NX4.0.0.

License requirements: None.

Scale

CustomSymbolData.Scale

Returns or sets the scale

-------------------------------------

Getter Method

Signature Scale()

Returns:Scale
Return type:float

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Scale(scale)

Parameters:scale (float) – New scale

New in version NX4.0.0.

License requirements: None.

ScaleExpression

CustomSymbolData.ScaleExpression

Returns or sets the scale expression

-------------------------------------

Getter Method

Signature ScaleExpression()

Returns:Scale expression
Return type:NXOpen.Expression

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScaleExpression(scaleExpression)

Parameters:scaleExpression (NXOpen.Expression) – New scale expression

New in version NX4.0.0.

License requirements: None.

SymbolPreferencesOption

CustomSymbolData.SymbolPreferencesOption

Returns or sets the symbol preferences option.

This option is only available when creating.

-------------------------------------

Getter Method

Signature SymbolPreferencesOption()

Returns:Symbol preferences option
Return type:NXOpen.Annotations.SymbolPreferencesOption

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymbolPreferencesOption(option)

Parameters:option (NXOpen.Annotations.SymbolPreferencesOption) – New symbol preferences option

New in version NX4.0.0.

License requirements: None.

TextPreferencesOption

CustomSymbolData.TextPreferencesOption

Returns or sets the text preferences option.

This option is only available when creating.

-------------------------------------

Getter Method

Signature TextPreferencesOption()

Returns:Text preferences option
Return type:NXOpen.Annotations.TextPreferencesOption

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature TextPreferencesOption(option)

Parameters:option (NXOpen.Annotations.TextPreferencesOption) – New text preferences option

New in version NX4.0.0.

License requirements: None.

Method Detail

Dispose

CustomSymbolData.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX4.0.0.

License requirements: None.

GetTextData

CustomSymbolData.GetTextData

Return the text data

Signature GetTextData()

Returns:List of text data objects
Return type:list of NXOpen.Annotations.CustomSymbolTextData

New in version NX4.0.0.

License requirements: None.

SetTextData

CustomSymbolData.SetTextData

Sets the text data

Signature SetTextData(data)

Parameters:data (list of NXOpen.Annotations.CustomSymbolTextData) – List of text data objects

New in version NX4.0.0.

License requirements: None.