SymbolPreferencesOption Enumeration

class NXOpen.Annotations.SymbolPreferencesOption

Bases: object

Specifies the custom symbol preferences for the following -

Crosshatch

Area fill

Color, font and line width

This option is only available when creating. Enum Members

Enum Member Enum Member Description
PartSymbol
Specifies part’s symbol preferences will be used
MasterSymbol
Specifies master symbol’s preferences will be used
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.