CircleCenterlineBuilder Class

class NXOpen.Annotations.CircleCenterlineBuilder

Bases: NXOpen.Annotations.CenterlineBuilder

Represents a CircleCenterline Builder

This is an abstract class.

Default values.

Property Value
Settings.Extension 6.35 (millimeters part), 0.25 (inches part)
Settings.Gap 1.5875 (millimeters part), 0.0625 (inches part)
Settings.IndividualDistance 0
Settings.Size 3.175 (millimeters part), 0.125 (inches part)
Settings.Width Thin

New in version NX6.0.0.

Properties

Property Description
FullCircle Returns or sets the method which returns full or partial circle flag
Inherit Returns the inherit object
Locations Returns the selction object of the centerline
Settings Returns the settings builder object for the centerline
Tag Returns the Tag for this object.
Type Returns or sets the method which returns type of centerline

Methods

Method Description
AddEndExtensions Adds extensions only at ends
AddExtension Adds extension based on select object index
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetAllExtensions Returns all extensions.
GetAllIndividualExtensions Returns individual extensions.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetEndExtensions Returns end extensions only.
GetObject Returns the object currently being edited by this builder.
RemoveEndExtensions Removes extensions only at ends
RemoveExtension Removes extension based on select object index
RemoveLocation Removes location object for a given index from the Select Object List.
ResetAllExtensions Reset all extensions by the supplied defaultValue
SetAllIndividualExtensions Sets all individual extensions
SetEndExtensions Modifies end extensions only
SetIndividualExtensions Modifies extensions based on select object index
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

CircleCenterlineBuilderTypes Enumeration the valid enumeration used for the creation types, applicable only while creation Once created type centerpoint will be set for all bolt circle/circular centerline

Property Detail

FullCircle

CircleCenterlineBuilder.FullCircle

Returns or sets the method which returns full or partial circle flag

-------------------------------------

Getter Method

Signature FullCircle()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FullCircle(fullType)

Parameters:fullType (bool) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Inherit

CircleCenterlineBuilder.Inherit

Returns the inherit object

-------------------------------------

Getter Method

Signature Inherit()

Returns:
Return type:NXOpen.SelectNXObject

New in version NX6.0.0.

License requirements: None.

Locations

CircleCenterlineBuilder.Locations

Returns the selction object of the centerline

-------------------------------------

Getter Method

Signature Locations()

Returns:
Return type:NXOpen.SelectNXObjectList

New in version NX6.0.0.

License requirements: None.

Settings

CircleCenterlineBuilder.Settings

Returns the settings builder object for the centerline

-------------------------------------

Getter Method

Signature Settings()

Returns:
Return type:NXOpen.Annotations.CircleCenterlineSettingsBuilder

New in version NX6.0.0.

License requirements: None.

Type

CircleCenterlineBuilder.Type

Returns or sets the method which returns type of centerline

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.Annotations.CircleCenterlineBuilderTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(method)

Parameters:method (NXOpen.Annotations.CircleCenterlineBuilderTypes) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

RemoveLocation

CircleCenterlineBuilder.RemoveLocation

Removes location object for a given index from the Select Object List.

This method is required for the retained circle centerline case , however the method can be used for removing any object from select object list for the Circle Centerline.

Signature RemoveLocation(index)

Parameters:index (int) – Index of the object in the select object list

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Validate

CircleCenterlineBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.