CircleCenterlineBuilderTypes Enumeration¶
NXOpen.Annotations.CircleCenterlineBuilder.Types is an alias for NXOpen.Annotations.CircleCenterlineBuilderTypes
-
class
NXOpen.Annotations.
CircleCenterlineBuilderTypes
¶ Bases:
object
the valid enumeration used for the creation types, applicable only while creation Once created type centerpoint will be set for all bolt circle/circular centerline
Enum Members
Enum Member Enum Member Description Through3Points Centerline using 3 or More Points MethodCenterpoint Centerline using Centerpoint Method-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-