AssociatedObjectsSetsBuilder Class¶
-
class
NXOpen.Annotations.
AssociatedObjectsSetsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
The associated objects sets builder is used to store lists of objects which annotations are associated to
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ObjectsSet1 | Returns the objects of set1 |
ObjectsSet2 | Returns the objects of set2 |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ObjectsSet1¶
-
AssociatedObjectsSetsBuilder.
ObjectsSet1
¶ Returns the objects of set1
-------------------------------------
Getter Method
Signature
ObjectsSet1()
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX10.0.0.
License requirements: None.
ObjectsSet2¶
-
AssociatedObjectsSetsBuilder.
ObjectsSet2
¶ Returns the objects of set2
-------------------------------------
Getter Method
Signature
ObjectsSet2()
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AssociatedObjectsSetsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.