AngularTolerance Class

class NXOpen.Annotations.AngularTolerance

Bases: NXOpen.TransientObject

Represents angular tolerance

New in version NX4.0.0.

Properties

Property Description
DimensionDecimalPlaces Returns or sets the number of decimal places for dimension
ToleranceType Returns or sets the tolerance type
ZeroToleranceDisplayStyle Returns or sets the zero tolerance display style

Methods

Method Description
Dispose Frees the object from memory.
GetLowerToleranceDegrees Returns the lower tolerance in degrees @return Lower tolerance in degrees
GetUpperToleranceDegrees Returns the upper tolerance in degrees @return Upper tolerance in degrees
SetLowerToleranceDegrees Sets the lower tolerance in degrees
SetUpperToleranceDegrees Sets the upper tolerance in degrees

Property Detail

DimensionDecimalPlaces

AngularTolerance.DimensionDecimalPlaces

Returns or sets the number of decimal places for dimension

-------------------------------------

Getter Method

Signature DimensionDecimalPlaces()

Returns:Number of dimension decimal places
Return type:int

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DimensionDecimalPlaces(dimensionDecimalPlaces)

Parameters:dimensionDecimalPlaces (int) – New number of dimension decimal places

New in version NX4.0.0.

License requirements: None.

ToleranceType

AngularTolerance.ToleranceType

Returns or sets the tolerance type

-------------------------------------

Getter Method

Signature ToleranceType()

Returns:Tolerance type
Return type:NXOpen.Annotations.ToleranceType

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ToleranceType(type)

Parameters:type (NXOpen.Annotations.ToleranceType) – New tolerance type

New in version NX4.0.0.

License requirements: None.

ZeroToleranceDisplayStyle

AngularTolerance.ZeroToleranceDisplayStyle

Returns or sets the zero tolerance display style

-------------------------------------

Getter Method

Signature ZeroToleranceDisplayStyle()

Returns:Zero tolerance display style
Return type:NXOpen.Annotations.ZeroToleranceDisplayStyle

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ZeroToleranceDisplayStyle(zeroDisplayStyle)

Parameters:zeroDisplayStyle (NXOpen.Annotations.ZeroToleranceDisplayStyle) –

New in version NX7.5.0.

License requirements: None.

Method Detail

Dispose

AngularTolerance.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX4.0.0.

License requirements: None.

GetLowerToleranceDegrees

AngularTolerance.GetLowerToleranceDegrees

Returns the lower tolerance in degrees

Signature GetLowerToleranceDegrees()

Returns:Lower tolerance in degrees
Return type:NXOpen.Annotations.Value

New in version NX4.0.0.

License requirements: None.

GetUpperToleranceDegrees

AngularTolerance.GetUpperToleranceDegrees

Returns the upper tolerance in degrees

Signature GetUpperToleranceDegrees()

Returns:Upper tolerance in degrees
Return type:NXOpen.Annotations.Value

New in version NX4.0.0.

License requirements: None.

SetLowerToleranceDegrees

AngularTolerance.SetLowerToleranceDegrees

Sets the lower tolerance in degrees

Signature SetLowerToleranceDegrees(lowerToleranceDegrees)

Parameters:lowerToleranceDegrees (NXOpen.Annotations.Value) – New lower tolerance in degrees

New in version NX4.0.0.

License requirements: None.

SetUpperToleranceDegrees

AngularTolerance.SetUpperToleranceDegrees

Sets the upper tolerance in degrees

Signature SetUpperToleranceDegrees(upperToleranceDegrees)

Parameters:upperToleranceDegrees (NXOpen.Annotations.Value) – New upper tolerance in degrees

New in version NX4.0.0.

License requirements: None.