/*
uf_udobj.h
File description:
The Open C API implementation of User Defined Objects (UDO's).
Please see the following for more documentation.
Overview
*****************************************************************************/
#ifndef UF_UDOBJ_H_INCLUDED
#define UF_UDOBJ_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <libufun_exports.h>
/*
**************************************************************************
*************************** '#define 's ***************************
**************************************************************************
*/
/* All of these may be used to test the status of the UDO; any bitwise or
combination of the lower three may be created to filter multiple cases.
For example, to determine if a link was removed either programmatically or
via normal delete, you would do the following:
( UF_UDOBJ_LINK_COUNT_DIFF | UF_UDOBJ_LINK_REMOVED )
*/
#define UF_UDOBJ_LINK_UPTODATE 0
#define UF_UDOBJ_LINK_COUNT_DIFF 1
#define UF_UDOBJ_LINK_CHANGED 2
#define UF_UDOBJ_LINK_REMOVED 4
/*
**************************************************************************
*************************** Structures ***************************
**************************************************************************
*/
typedef unsigned int UF_UDOBJ_class_t;
struct UF_UDOBJ_link_s {
int link_type; /* the link type to create; any of
these possibilities:
Link type 1 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
UDO is also deleted; if the
associated object is updated the
UDO is updated
Link type 2 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is deleted; if the
UDO is updated the associated NX
object is unaffected; if the
associated object is deleted, it
is left in the data model in a
condemned state and remains
attached to the UDO; if the
associated object is updated
the UDO is unaffected
Link type 3 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
link to the UDO is removed and
the UDO is updated; if the
associated object is updated the
UDO is updated
Link type 4 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
link to the UDO is removed and
the UDO is unaffected; if the
associated object is updated the
UDO is unaffected
*/
tag_t assoc_ug_tag; /* In most cases this will be the
NX tag to associate the UDO
with. However for the routine
UF_UDOBJ_ask_udo_links_to_obj,
this will return the tag of the
UDO that the object is linked
to.
*/
unsigned int object_status; /* the up-to-date indicator for
the object associated with
the UDO
0 = Up to date
1 = Out of date
*/
} ;
typedef struct UF_UDOBJ_link_s UF_UDOBJ_link_t , *UF_UDOBJ_link_p_t;
struct UF_UDOBJ_all_data_s {
UF_UDOBJ_class_t class_id; /* the class identifier for the
UDO
*/
unsigned int udo_status; /* the out-of-date indicator for
the UDO
*/
unsigned int num_ints; /* the number of integers in the
UDO
*/
int *ints; /*
the integers in the UDO --
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
unsigned int num_doubles; /* the number of doubles in the
UDO
*/
double *doubles; /*
the doubles in the UDO --
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
unsigned int num_strings; /* the number of strings in the
UDO
*/
char **strings; /*
the strings in the UDO --
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
unsigned int num_links; /* the number of links in the UDO
*/
UF_UDOBJ_link_t *link_defs; /*
the link types and the
associated NX objects in the
UDO -- NOTE: this is
allocated memory that needs
to be freed when no longer
needed . See
UF_UDOBJ_free_udo_data
*/
unsigned int num_lengths; /* the number of lengths in the
UDO
*/
double *lengths; /*
The length data in the UDO.
These doubles will be marked
as measurements of length, so
that conversion from metric to
english units will properly
work.
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
unsigned int num_areas; /* the number of areas in the UDO
*/
double *areas; /*
The area data in the UDO --
These doubles will be marked
as measurements of area, so
that conversion from metric to
english units will properly
work.
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
unsigned int num_volumes; /* the number of volumes in the
UDO
*/
double *volumes; /*
the volume data in the UDO --
These doubles will be marked
as measurements of volume, so
that conversion from metric to
english units will properly
work.
NOTE: this is allocated memory
that needs to be freed when no
longer needed. See
UF_UDOBJ_free_udo_data
*/
} ;
typedef struct UF_UDOBJ_all_data_s UF_UDOBJ_all_data_t , *UF_UDOBJ_all_data_p_t;
/*
**************************************************************************
******************* Function Pointer 'typedef's ******************
**************************************************************************
*/
typedef void (*UF_UDOBJ_attn_pt_f_t) (
tag_t udo_tag, /* <I> -- the tag for the UDO
whose attention point
is being defined
*/
void *display_context /* <I> -- a pointer to a private
structure used in
display calls
*/
);
typedef void (*UF_UDOBJ_delete_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
who has an associated
object being deleted
*/
UF_UDOBJ_link_p_t deleted_obj /* <I> -- the link for the item
that is deleted
*/
);
typedef void (*UF_UDOBJ_display_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
being displayed
*/
void *display_context /* <I> -- a pointer to a private
structure used in
display calls
*/
);
typedef void (*UF_UDOBJ_fit_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
being fit to the view
*/
void *display_context /* <I> -- a pointer to a private
structure used in
fit calls
*/
);
typedef void (*UF_UDOBJ_screen_size_fit_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO whose screen-size
objects need to be fit to the view
*/
void *display_context /* <I> -- a pointer to a private
structure used in
screen-size-fit calls
*/
);
typedef void (*UF_UDOBJ_info_obj_f_t) (
tag_t udo_tag /* <I> -- the tag for the UDO
for which information
is being requested
*/
);
typedef void (*UF_UDOBJ_select_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
being selected
*/
void *display_context /* <I> -- a pointer to a private
structure used in
selection calls
*/
);
typedef void (*UF_UDOBJ_update_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
being updated
*/
UF_UDOBJ_link_p_t update_cause /* <I> -- the link for the item
that caused the UDO to be
updated
*/
);
typedef void (*UF_UDOBJ_is_occurrenceable_f_t) (
tag_t udo_tag , /* <I> -- the tag for the UDO
being fit to the view
*/
logical *is_occurrenceable /* <O> -- TRUE if object can
be occurrenced otherwise
FALSE
*/
);
typedef void (*UF_UDOBJ_edit_f_t) (
tag_t udo_tag /* <I> -- the tag for the UDO
which is being edited in the callback
*/
);
typedef void (*UF_UDOBJ_suppress_f_t) (
tag_t udo_feat_tag /* <I> -- the tag for the UDO feature
which is being suppressed in the callback
*/
);
/*
The default behavior is not to allow selection of owned objects. If you pick
an owned object, the UDO object is actually selected. If the owning UDO
object is not eligible to be selected, then the owned object can not be
picked.
The UDO can be changed to allow the selection of an owned object. In this
case picking of the owned object will select the owned object and activate
the up one level button, if the owning UDO is eligible for selection. Now
the owning UDO can be selected using this button. If the UDO is not eligible
for selection, picking of the owned object will select the owned object only.
The selection behavior of the UDO class can be changed by using the routine:
UF_UDOBJ_set_owned_object_selection
UDO's can own other UDO's. So you can have the chain:
UDO1 owns UDO2 owns UDO3 owns point1
For a detailed discussion, please see Selection of UDO's that own other UDO's
Interactively selecting owned objects for deletion is specifically disabled.
So even if the UDO class is set for UF_UDOBJ_ALLOW_SELECTION, owned objects
can not be interactively selected for delete through Edit->delete.
If the owned object is a solid, then the solid may still be selected through
modeling selection where a feature list is presented to the user. So for
example, it may be deleted through Edit->Feature->Delete Feature. This is
because ultimately modeling is in control of all solid bodies.
*/
enum UF_UDOBJ_owned_object_selection_e
{
UF_UDOBJ_DONT_ALLOW_SELECTION = 1, /* Owned objects can not be selected.
Selection of the owned object results in
the UDO being selected. If the UDO is
not selectable, the owned object will not
be eligible for selection. */
UF_UDOBJ_ALLOW_SELECTION = 2 /* Owned objects can be selected. If the
UDO is selectable, then selecting the
owned object will select it and activate
the Up One Level button. If the UDO is
not selectable, then the owned object may
be selected. */
};
typedef enum UF_UDOBJ_owned_object_selection_e UF_UDOBJ_owned_object_selection_t;
enum UF_UDOBJ_query_class_id_e
{
UF_UDOBJ_DONT_ALLOW_QUERY_CLASS_ID = 1, /* The class id can not be found by the name. */
UF_UDOBJ_ALLOW_QUERY_CLASS_ID = 2 /* Given the name of the class, the class id
can be found using UF_UDOBJ_ask_class_id_of_name */
};
typedef enum UF_UDOBJ_query_class_id_e UF_UDOBJ_query_class_id_t;
/*
**************************************************************************
****************** Functions Relating to Classes *****************
**************************************************************************
*/
/* ******************** Class Creation ******************** */
/******************************************************************************
Creates the class, given a class name, and friendly name for a
particular type of UDO. Returns a class identifier which is used by
UF_UDOBJ_create_udo to create the UDO and return its tag.
UF_UI_add_to_class_sel can be used to enable the friendly name on the
class selection dialog.
Environment: Internal and External
See Also: UF_UI_add_to_class_sel
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_create_class (
const char * class_name ,/* <I>
The class name for the particular type of User
Defined Object.
*/
const char * friendly_name ,/* <I>
A user-friendly name that appears in the class
selection dialog (if enabled) and in other
locations where a name is useful.
*/
UF_UDOBJ_class_t * class_id /* <O>
The class identifier. This identifier is not
persistent across NX sessions nor is it stored in
NX part files.
*/
);
/* ******************** Class Querying ******************** */
/*******************************************************************************
Finds both the class name and the user friendly name for the specified
class identifier. The friendly_name appears in the class selection dialog
if it is enabled.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_class_data (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created class.
*/
char ** class_name ,/* <OF>
The name of the class of UDOs. Use UF_free to
deallocate memory when done.
*/
char ** friendly_name /* <OF>
The user-friendly class name. Use UF_free to
deallocate memory when done.
*/
);
/* ******************** Class Methods ******************** */
/******************************************************************************
Registers the attention point function (method) to call when the
UDOs with the input class identifier pass through the attention point
computation event. The attention point is a temporary display point
near an object that is used during particular NX events. For
example, during Info-->Object a temporary number is placed near the
object. NX calculates the location for the attention point
based on the primitives used in constructing the UDO.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_attn_pt_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_attn_pt_f_t attn_pt_func /* <I>
The function to invoke when UDOs for this
class pass through attention point
computations.
*/
);
/******************************************************************************
Register's the delete function (method) to call when a UDO with a
type 2 or 3 linked object associated to the UDO passes through
delete. Objects associated to the UDO with a type 1 link do not
invoke the method because the UDO is deleted when its associated
object is deleted. Objects associated to a UDO with a UDO owning
link do not cause the method to be invoked because the associated
object can not be deleted directly.
The following restrictions apply:
. The callback routine must not call UF_MODL_update.
. No Features may be deleted from this callback.
. The work part must not be changed.
This callback should not call any functions that change the work or displayed
part. This includes functions that change the work part as part of their
operation, such as UF_PART_import.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_delete_cb(
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_delete_f_t delete_func /* <I>
The function to invoke when objects associated
to UDOs in this class pass through delete.
*/
);
/******************************************************************************
Registers the display function (method) to call when the UDOs with
the input class identifier pass through the display event.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_display_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_display_f_t display_func /* <I>
The function to invoke when UDOs for this
class pass through the display.
*/
);
/******************************************************************************
Registers the fit function (method) to call when the UDOs with the
input class identifier pass through the fit into view event. NX
calculates the extents of clipping required based on the primitives
used in the UDO's construction.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_fit_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_fit_f_t fit_func /* <I>
The function to invoke when UDOs for this
class pass through fit to the view display code.
*/
);
/******************************************************************************
Registers the screen size fit function (method) to call when the UDOs with the
input class identifier pass through the add screen size objects to fit into view event.
"Screen Size Fit" applies to primitives whose size remains the same on the screen
regardless of the scale of the view. The size of other primitives on the screen
changes as the view scale changes. NX calculates the extents of clipping required
based on the screen size primitives used in the UDO's construction.
You should only call this function if your UDO contains geometry which can
participate in "Screen Size Fit." As of NX 8.0, this is only ScreenStandardText
and AbsoluteRotationScreenSizeText, which are available in class NX/Open class
UserDefinedObjects::UserDefinedObjectDisplayContext.
Environment: Internal and External
See Also:
History: NX 8.0
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_screen_size_fit_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_screen_size_fit_f_t screen_size_fit_func /* <I>
The function to invoke when UDOs for this class pass
through add screen size objects to fit to the view display code.
*/
);
/******************************************************************************
Registers the Info-->Object method to call when the UDOs with the
input class identifier are queried interactively in NX with the
Info-->Object menu option. It is safe to register a method in external
mode, but Info-->Object functionality is only available in internal
mode.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_info_obj_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier for which to register the
Info-->Object method.
*/
UF_UDOBJ_info_obj_f_t info_object_method /* <I>
The method to use in interactive NX
when you invoke Info-->Object on a
UDO of this class.
*/
);
/******************************************************************************
Registers the select function (method) to call when the UDOs with
the input class identifier pass through the selection event. This UDO
callback informs NX of the extents of the UDO via the
display primitives, then NX's internal algorithms decide to
select the UDO or not. UF_UI_add_to_class_sel can be used to enable
the friendly name on the class selection dialog.
Environment: Internal and External
See Also: UF_UI_add_to_class_sel
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_select_cb(
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_select_f_t select_func /* <I>
The function to invoke when UDOs for this
class pass through selection.
*/
);
/******************************************************************************
Registers the update function (method) to call when the UDOs with
the input class identifier pass through the update event. The method is
called when a UDO with either a link type 1 or a link type 3
association to it passes through update. Link type 2 and the UDO
owning link do not invoke the method because objects associated to
UDOs with link type 2 and UDO owning links do not add the UDOs
to the update list, by definition.
While within the update callback, you may freely query the data
model. You may also edit the free form data areas in the UDO.
Additionally, you may display a dialog (in internal Open API) to
inform the NX user of the affect the edit may have on the
UDO.
This callback should not call any functions that change the work or displayed
part. This includes functions that change the work part as part of their
operation, such as UF_PART_import.
Note that if an object you are linked to (with a type 1 or a type 3 link) is
deleted, the UDO update method will be called. If your update method does
nothing, you will remain linked to a condemned object, and you must take that
into account when you try to use the linked object. If you want, your update
method can loop over all linked objects, calling UF_OBJ_ask_status, if you
are linked to an object that has a status of UF_OBJ_CONDEMNED, then the update
method can decide what is the appropriate action to take.
The following restrictions apply:
. The update process must not be explicitly invoked again with UF_MODL_update.
. The work part must not be changed.
. No Features may be deleted from this callback.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_update_cb(
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_update_f_t update_func /* <I>
The function to invoke when UDOs for this
class pass through update.
*/
);
/******************************************************************************
Registers the function (method) which determines if this UDO is occurrenceable.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_is_occurrenceable_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_is_occurrenceable_f_t is_occurrenceable_func /* <I>
The function to invoke to determine if this UDO
should be occurrenceable.
*/
);
/******************************************************************************
Registers the function (method) which is invoked when editing this UDO.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_edit_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_edit_f_t edit_func /* <I>
The function to invoke when editing the UDO.
*/
);
/******************************************************************************
Registers the function (method) which is invoked when suppressing this UDO feature.
Note this method is not called unless you have a UDO FEATURE. Also it *may* not
get called when the system automatically suppresses the feature during update.
Also note the user should call UF_MODL_ask_suppress_feature() in their callback to
see if the input udo feature is currently getting suppressed or unsuppressed.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_register_suppress_cb (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
UF_UDOBJ_suppress_f_t suppress_func /* <I>
The function to invoke when suppressing or unsuppressing the UDO feature.
*/
);
/*
**************************************************************************
******************* Functions Relating to UDOs *******************
**************************************************************************
*/
/* ******************** UDO Creation ******************** */
/******************************************************************************
Creates a UDO of the class specified by the input class identifier. This
creates a UDO "template" with a name and status. Note that creating a UDO
will not display the UDO. This is so that you can add data that your display
routines may need prior to the UDO being displayed. When the UDO has been
fully created, call UF_DISP_add_item_to_display to actually display the UDO.
Environment: Internal and External
See Also:
See Also: UF_DISP_add_item_to_display
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_create_udo (
UF_UDOBJ_class_t class_id ,/* <I>
The class identifier from a previously created
class.
*/
tag_t * udo_tag /* <O>
The tag for the UDO
*/
);
/******************************************************************************
Creates both a UDO object and a UDO feature from an existing
class identifier. Note that UF_MODL_update() must be called to complete the
creation of the UDO feature and have it appear in the Model Navigation Tool.
Environment: Internal & External
See Also:
History: This function was originally released in V15.0.
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_create_udo_feature (
UF_UDOBJ_class_t class_id , /* <I>
The class identifier from
a previously created class
*/
tag_t *udo_tag , /* <O>
The tag for the UDO
*/
tag_t *udo_feature_tag /* <O>
The tag for the UDO feature
*/
);
/*******************************************************************************
Creates a UDO feature associated with a UDO object and returns
the tag of the newly created feature. This function returns an error if
you attempt to create a UDO feature for a UDO object which is
already associated to a UDO feature.
Environment: Internal & External
See Also:
History: This function was originally released in V15.0.
*******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_create_udo_feature_from_udo (
tag_t udo_tag , /* <I>
The UDO to create the UDO
feature from
*/
tag_t *udo_feature_tag /* <O>
The newly created UDO feature
*/
);
/******************************************************************************
Edits a UDO feature by replacing the existing tag of the UDO object
with the input tag of the UDO object. The old UDO object is no
longer associated to a UDO feature and may be associated to
another UDO feature. If the input UDO object is associated to
another UDO feature, the editing is not done and this routine
returns an error.
Environment: Internal & External
See also:
History: This function was originally released in V15.0
*******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_udo_of_udo_feature (
tag_t udo_feature_tag , /* <I>
The UDO feature to edit.
*/
tag_t udo_tag /* <I>
The UDO to edit the UDO
feature with
*/
);
/* ******************** UDO Appending ******************** */
/******************************************************************************
Adds integers to the free form data area of an UDO. Any number of
valid integer elements can be added. These calls are cumulative, if you
make one call to add two integers, and then a second call to add three
integers, you will end up with 5 integers on the UDO, and UF_UDOBJ_edit_integers
would expect you to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_integers
UF_UDOBJ_delete_integers
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_integers (
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_ints ,/* <I>
The number of integers to add.
*/
int * ints /* <I>
The integers to add to the UDO.
*/
);
/******************************************************************************
Adds doubles to the free form data area of an UDO. Any number of
valid double elements can be added. These calls are cumulative, if you
make one call to add two doubles, and then a second call to add three
doubles, you will end up with 5 doubles on the UDO, and UF_UDOBJ_edit_doubles
would expect you to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_doubles
UF_UDOBJ_delete_doubles
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_doubles(
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_doubles ,/* <I>
The number of doubles to add.
*/
double * doubles /* <I>
The doubles to add to the UDO.
*/
);
/******************************************************************************
Adds strings to the free form data area of an UDO. Any number of
valid null terminated string elements can be added. These calls are cumulative,
if you make one call to add two strings, and then a second call to add three
strings, you will end up with 5 strings on the UDO, and UF_UDOBJ_edit_strings
would expect you to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_strings
UF_UDOBJ_delete_strings
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_strings(
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_strings ,/* <I>
The number of strings to add.
*/
char * strings[] /* <I>
The strings to add to the UDO.
*/
);
/******************************************************************************
Adds a link to the specified NX objects defined by the
link_defs[ ] array.
Links cannot be cyclical. Also, a type 2 link cannot be used to link
UDOs to features, solid faces, or solid edges. You can only link to
objects found in uf_object_types.h. These calls are cumulative, if
you make one call to add two links, and then a second call to add three
links, you will end up with 5 links on the UDO, and UF_UDOBJ_edit_links
would expect you to pass in 5 elements.
The order in which NX objects are passed into this routine is NOT preserved.
So, no assumptions should be made in this regard.
Environment: Internal and External
See Also: UF_UDOBJ_edit_links
UF_UDOBJ_delete_link
UF_UDOBJ_link_t
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_links (
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_links ,/* <I>
The number of objects to link to the UDO.
*/
UF_UDOBJ_link_t link_defs[] /* <I>
The link types and the associated NX objects to
link to.
*/
);
/******************************************************************************
Adds objects by owning links to a UDO. These calls are cumulative, if
you make one call to add two links, and then a second call to add three
links, you will end up with 5 links on the UDO.
If the udo_tag is a UDO Feature, then the array of input tags can not include
any solids, faces, edges, sheets or features. The array of tags should only
be wireframe data.
The order in which NX objects are passed into this routine is NOT preserved.
So, no assumptions should be made in this regard.
Environment: Internal and External
See Also: UF_UDOBJ_delete_owning_link
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_owning_links (
tag_t udo_tag ,/* <I>
The tag of the UDO to which to add owning links.
*/
unsigned int num_links ,/* <I>
The number of objects to link to the UDO by owning
links.
*/
tag_t ug_objs[] /* <I>
An array of tags of objects to link to the UDO by owning links.
*/
);
/*****************************************************************************
Adds length data to the convertible data area. Any number of doubles
can be added to the lengths array. Each double represents a unit of
length. These calls are cumulative, if you make one call to add two
lengths, and then a second call to add three lengths, you will end up
with 5 lengths on the UDO, and UF_UDOBJ_edit_lengths would expect you
to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_lengths
UF_UDOBJ_delete_lengths
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_lengths (
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_lengths ,/* <I>
The number of lengths to add.
*/
double * lengths /* <I>
The length data to add to the UDO.
*/
);
/*******************************************************************************
Adds area data to the convertible data area. Any number of doubles
can be added to the areas array. Each double represents a unit of
area. These calls are cumulative, if you make one call to add two
areas, and then a second call to add three areas, you will end up
with 5 areas on the UDO, and UF_UDOBJ_edit_areas would expect you
to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_areas
UF_UDOBJ_delete_areas
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_areas (
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_areas ,/* <I>
The number of areas to add.
*/
double * areas /* <I>
The area data to add to the UDO.
*/
);
/******************************************************************************
Adds volume data to the convertible data area. Any number of
doubles can be added to the volumes array. Each double represents a
unit of volume. These calls are cumulative, if you make one call to add two
volumes, and then a second call to add three volumes, you will end up
with 5 volumes on the UDO, and UF_UDOBJ_edit_areas would expect you
to pass in 5 elements.
Environment: Internal and External
See Also: UF_UDOBJ_edit_volumes
UF_UDOBJ_delete_volumes
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_add_volumes(
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
unsigned int num_volumes ,/* <I>
The number of volumes to add.
*/
double * volumes /* <I>
The volume data to add to the UDO.
*/
);
/* ******************** UDO Querying ******************** */
/******************************************************************************
Finds all of the data associated with an UDO and returns it in the
data structure UF_UDOBJ_all_data_s. The order of the links returned by this
routine need not match with the order in which they are created through
UF_UDOBJ_add_links or UF_UDOBJ_add_owning_links. No assumptions should be made
in this regard.
Environment: Internal and External
See Also: UF_UDOBJ_free_udo_data
UF_UDOBJ_add_links
UF_UDOBJ_add_owning_links
UF_UDOBJ_all_data_t
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_udo_data (
tag_t udo_tag ,/* <I>
The tag for the UDO
*/
UF_UDOBJ_all_data_t *all_data /* <OF>
All of the data associated with the UDO. The
structure that this points to becomes fully
populated following this call. Certain structure
members must be freed when no longer needed.
This can be freed by calling
UF_UDOBJ_free_udo_data
*/
);
/******************************************************************************
Frees all of the data that was dynamically allocated to the address of
the UF_UDOBJ_all_data_s structure. This structure is populated with
data after a call by UF_UDOBJ_ask_udo_data .
Environment: Internal and External
See Also: UF_UDOBJ_ask_udo_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_free_udo_data (
UF_UDOBJ_all_data_p_t all_data /* <I>
A structure previously populated by
UF_UDOBJ_ask_udo_data. This function frees
all the data dynamically allocated by that
function.
*/
);
/******************************************************************************
Finds the class name associated with the UDO.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_udo_class_name (
tag_t udo_tag ,/* <I>
Tag for the UDO.
*/
char ** udo_class_name /* <OF>
The class name assigned to the UDO. Ensure
the memory is freed using UF_free once the
information is no longer needed.
*/
);
/******************************************************************************
Finds the class id associated with the given class name.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_class_id_of_name (
const char *class_name, /* <I> Name of a udo class - NOTE: do not use the
"friendly" class name */
UF_UDOBJ_class_t *class_id /* <O> Class id associated with the given class name */
);
/******************************************************************************
Queries whether UDOs reference the specified NX object.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_is_obj_linked_to_udo(
tag_t ug_tag ,/* <I>
The tag of the NX object to query as to
whether UDOs reference it or not.
*/
logical * linked /* <O>
TRUE = UDOs reference NX object
FALSE = UDOs do not reference NX object.
*/
);
/******************************************************************************
Queries if an NX object has an owning link by a UDO.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_is_owned (
tag_t obj_tag ,/* <I>
The tag of the NX object to query
*/
logical * owned /* <O>
TRUE = NX Object has an owning link to a UDO.
FALSE = No owning link
*/
);
/******************************************************************************
Queries if the specified NX object is linked to a UDO by an owning
link. Returns the tag of the UDO with the owning link. Returns
NULL_TAG if there is no UDO with an owning link to the specified
NX object.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_owning_udo (
tag_t obj_tag ,/* <I>
The tag of the NX object to query
*/
tag_t* udo_tag /* <O>
The tag of the UDO which has an owning link
to the specified NX object.
*/
);
/******************************************************************************
Queries the number of associated NX objects that have owning links
to the specified UDO.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_owned_objects (
tag_t udo_tag ,/* <I>
The tag of the UDO to query
*/
int* num_owned_objects ,/* <O>
The number of NX objects linked to the UDO
by owning links.
*/
tag_t** owned_objects /* <OF>
An array of tags of NX objects linked to the
UDO by owning links.
*/
);
/******************************************************************************
Finds all of the UDO links to a particular NX object.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_udo_links_to_obj (
tag_t ug_tag ,/* <I>
The tag of the NX object for which to retrieve
the UDO links.
*/
int * num_links ,/* <O>
The number of UDO links associated with the
NX object.
*/
UF_UDOBJ_link_t ** udo_links /* <OF>
The links between UDOs and the NX object.
Note that the member element
udo_links[i].assoc_ug_tag will be the tag of
the i+1 UDO that links to this object.
When done, use UF_free to deallocate memory
for these links.
*/
);
/*****************************************************************************
Inquires whether a feature is a UDO feature.
Environment: Internal & External
See Also:
History:This function was originally released in V15.0.
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_is_udo_feature(
tag_t feature_tag, /* <I>
the feature to check
*/
logical *is_udo_feature /* <O>
TRUE if a UDO feature else FALSE
*/
);
/******************************************************************************
Inquires the UDO feature tag of the input UDO object. A UDO
object may have only one UDO feature associated to it.
Environment: Internal & External
See Also:
History: This function was originally released in V15.0.
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_udo_feature_of_udo(
tag_t udo_tag, /* <I>
The tag of the UDO object whose
feature we are returning.
*/
tag_t *udo_feature_tag /* <O>
The tag of the UDO feature of
the input object. NULL_TAG will
be returned if there is no UDO
feature for the input object.
*/
);
/******************************************************************************
Inquires the tag of the UDO object that is associated to the input
UDO feature
Environment: Internal & External
See Also:
History: This function was originally released in V15.0.
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_ask_udo_of_udo_feature(
tag_t udo_feature_tag, /* <I>
The tag of the UDO feature whose
UDO object we are returning.
*/
tag_t *udo_tag /* <O>
The tag of the UDO object of the
input object.
*/
);
/* ******************** UDO Editing ******************** */
/*****************************************************************************
Clears the out-of-date indicator of an UDO.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_clear_udo_status (
tag_t udo_tag /* <I>
Tag for the UDO whose out-of-date indicator
is to be cleared.
*/
);
/*****************************************************************************
Clears the link status of a UDO.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_clear_link_status (
tag_t udo_tag ,/* <I>
The tag of the UDO whose link's status is to be cleared.
*/
UF_UDOBJ_link_p_t link_to_clear /* <I>
The link whose status is to be cleared.
*/
);
/*****************************************************************************
Edits the free form integer area of a UDO. The input array must have elements
for all of the integers currently on the UDO. You should know the data model
for your UDO, but if you are unsure of the number of integers on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_integers
UF_UDOBJ_add_integers
UF_UDOBJ_ask_udo_data
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_integers(
tag_t udo_tag ,/* <I>
The tag of the UDO whose integers are to be edited.
*/
int integers[] /* <I>
The new integers for the UDO.
*/
);
/*****************************************************************************
Edits the free form double area of a UDO. The input array must have elements
for all of the doubles currently on the UDO. You should know the data model
for your UDO, but if you are unsure of the number of doubles on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_doubles
UF_UDOBJ_add_doubles
UF_UDOBJ_ask_udo_data
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_doubles (
tag_t udo_tag ,/* <I>
The tag of the UDO whose doubles are to be edited.
*/
double doubles[] /* <I>
The new doubles for the UDO.
*/
);
/*****************************************************************************
Edits the free form string area of a UDO. The input array must have elements
for all of the strings currently on the UDO. You should know the data model
for your UDO, but if you are unsure of the number of strings on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_strings
UF_UDOBJ_add_strings
UF_UDOBJ_ask_udo_data
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_strings (
tag_t udo_tag ,/* <I>
The tag of the UDO whose strings are to be edited.
*/
char * strings[] /* <I>
The new strings for the UDO.
*/
);
/*****************************************************************************
Edits the lengths convertible data area of a UDO. The input array must have
elements for all of the lengths currently on the UDO. You should know the data
model for your UDO, but if you are unsure of the number of lengths on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_lengths
UF_UDOBJ_add_lengths
UF_UDOBJ_ask_udo_data
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_lengths (
tag_t udo_tag ,/* <I>
The tag of the UDO whose lengths are to be edited.
*/
double lengths[] /* <I>
The new lengths for the UDO.
*/
);
/*****************************************************************************
Edits the areas convertible data area of a UDO. The input array must have
elements for all of the areas currently on the UDO. You should know the data
model for your UDO, but if you are unsure of the number of areas on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_areas
UF_UDOBJ_add_areas
UF_UDOBJ_ask_udo_data
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_areas (
tag_t udo_tag ,/* <I>
The tag of the UDO whose areas are to be edited.
*/
double areas[] /* <I>
The new areas for the UDO.
*/
);
/*****************************************************************************
Edits the volumes convertible data area of a UDO. The input array must have
elements for all of the volumes currently on the UDO. You should know the data
model for your UDO, but if you are unsure of the number of volumes on a UDO,
UF_UDOBJ_ask_udo_data will return this information.
Environment: Internal and External
See Also: UF_UDOBJ_delete_volumes
UF_UDOBJ_add_volumes
UF_UDOBJ_ask_udo_data
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_volumes (
tag_t udo_tag ,/* <I>
The tag of the UDO whose volumes are to be edited.
*/
double volumes[] /* <I>
The new volumes for the UDO.
*/
);
/*****************************************************************************
Edits a UDO's link with the following edit features:
Replaces all the links for a specific link type within a UDO for a
particular NX object with another NX object.
Only affects a single link type at a time. Therefore, if there are
multiple links within a UDO to the same object, each with separate
link types, this function must be used once for each link type.
If there are multiple links to the same NX object with the same
link type, all the links are affected.
Environment: Internal and External
See Also: UF_UDOBJ_ask_udo_data
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_link (
tag_t udo_tag ,/* <I>
The tag of the UDO whose link is to be edited.
*/
UF_UDOBJ_link_p_t link_to_edit ,/* <I>
The link within the UDO whose reference is to
be changed.
*/
tag_t new_assoc_ug_tag /* <I>
The tag to insert into the link in place of the tag
currently in use.
*/
);
/*****************************************************************************
Edit the link records of a UDO. The input array should contain all of
the link records of the UDO. The edit will start at location
link_defs[start_location] and continue for count elements of the array.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_edit_links (
tag_t udo_tag , /* <I>
The tag of the UDO whose links
are to be edited
*/
const UF_UDOBJ_link_t *link_def, /* <I>
The new links for the UDO
*/
unsigned int start_location , /* <I>
The location in the link_defs
array where editing is to begin
(This should be a "C" based array
index.)
*/
unsigned int count /* <I>
The count of links to be edited
from start_location
*/
);
/******************************************************************************
Deletes the free form integer area of a UDO starting at the
designated location and concluding with the specified numbers of
integers to delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_integers
UF_UDOBJ_edit_integers
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_integers (
tag_t udo_tag ,/* <I>
The tag of the UDO whose integers are to be deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO integer area to
start deleting from. Valid values are 1 through
the number of integers in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of integers to delete.
*/
);
/******************************************************************************
Deletes the free form doubles area of a UDO starting at the
designated location and concluding with the specified numbers of
doubles to delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_doubles
UF_UDOBJ_edit_doubles
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_doubles (
tag_t udo_tag ,/* <I>
The tag of the UDO whose doubles are to be
deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO double area to
start deleting from. Valid values are 1 through
the number of doubles in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of doubles to delete.
*/
);
/******************************************************************************
Deletes the free form strings area of a UDO starting at the designated
location and concluding with the specified numbers of strings to
delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_strings
UF_UDOBJ_edit_strings
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_strings (
tag_t udo_tag ,/* <I>
The tag of the UDO whose strings are to be
deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO string area to
start deleting from. Valid values are 1 through
the number of strings in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of strings to delete.
*/
);
/******************************************************************************
Deletes a UDO's link.
Environment: Internal and External
See Also: UF_UDOBJ_add_links
UF_UDOBJ_edit_links
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_link (
tag_t udo_tag ,/* <I>
The tag of the UDO whose link is to be
deleted.
*/
UF_UDOBJ_link_p_t link_to_delete /* <I>
The link to delete from the UDO.
*/
);
/*****************************************************************************
Deletes the owning link between a UDO and its associated NX
object.
Environment: Internal and External
See Also: UF_UDOBJ_add_owning_links
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_owning_link (
tag_t udo_tag ,/* <I>
The tag UDO whose owning link is to be
deleted.
*/
tag_t ug_tag /* <I>
The tag of the NX object whose UDO owning
link is to be deleted.
*/
);
/*****************************************************************************
Deletes the convertible lengths area of a UDO starting at the
designated location and concluding with the specified numbers of
lengths to delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_lengths
UF_UDOBJ_edit_lengths
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_lengths (
tag_t udo_tag ,/* <I>
The tag of the UDO whose lengths are to be
deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO length area to
start deleting from. Valid values are 1 through
the number of lengths in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of lengths to delete.
*/
);
/*****************************************************************************
Deletes the convertible areas area of a UDO starting at the
designated location and concluding with the specified numbers of
areas to delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_areas
UF_UDOBJ_edit_areas
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_areas (
tag_t udo_tag ,/* <I>
The tag of the UDO whose areas are to be
deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO area values to
start deleting from. Valid values are 1 through
the number of areas in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of areas to delete.
*/
);
/*****************************************************************************
Deletes the convertible volumes area of a UDO starting at the
designated location and concluding with the specified numbers of
volumes to delete.
Environment: Internal and External
See Also: UF_UDOBJ_add_volumes
UF_UDOBJ_edit_volumes
History:
****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_delete_volumes(
tag_t udo_tag ,/* <I>
The tag of the UDO whose volumes are to be
deleted.
*/
unsigned int start_loc ,/* <I>
The location within the UDO volume area to
start deleting from. Valid values are 1 through
the number of volumes in the UDO.
*/
unsigned int num_to_delete /* <I>
The numbers of volumes to delete.
*/
);
/* ******************** UDO Cycling ******************** */
/*****************************************************************************
Cycles the UDOs in the part with the specified input tag. Input a
NULL_TAG to start the cycle. The cycle ends when a NULL_TAG
is returned.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_cycle_udos_by_class (
tag_t part_tag ,/* <I>
The part in which to cycle UDOs.
*/
UF_UDOBJ_class_t class_id ,/* <I>
The UDO class to cycle.
*/
tag_t * udo_tag /* <I/O>
The UDO found. The cycle starts and ends with
a NULL_TAG. The tag from the previous cycle
should be input for the next cycle.
*/
);
/* ******************** UDO Versioning ******************** */
/*******************************************************************************
Assigns an existing UDO to a new class id so that it can adopt the
callback/behaviors of the new class.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_version_udo(
tag_t udo_tag ,/* <I>
Tag of the UDO whose class you wish to
change.
*/
UF_UDOBJ_class_t class_id /* <I>
The udo will now belong in this class.
*/
);
/*****************************************************************************
Explicitly log the UDO feature for update. This may be called for edits that
do not implicitly log the UDO feature. UF_UDOBJ_edit_integers(), for example,
does not cause the UDO feature to be logged for update. If you consider the
UDO to be out of date, call this routine and then call UF_MODL_update().
Environment : Internal and External
See Also:
History: Originally released in V16.0
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_log_udo_feature_for_update
(
tag_t udo_feature_tag /* <I> The UDO feature to log for update */
);
/*****************************************************************************
Set the behavior of selection of owned objects for the UDO class. The
default selection mode is UF_UDOBJ_DONT_ALLOW_SELECTION. This means that an
owned object can not be selected independently.
Setting the selection of owned objects to UF_UDOBJ_ALLOW_SELECTION means that
if an owned object and the UDO are both selectable, selecting the owned object
will result in the owned NX Object being selected and Up One Level button
activated, in interactive selection. If the UDO is not selectable selection of
the owned object would still be possible.
You may want to set UF_UDOBJ_ALLOW_SELECTION when your UDO contains only one
owned object, and you want to inherit the characteristics of that object. For
instance if your owned object is a spline, which your UDO computes the knot
points for, you may want the spline to be selectable by modeling operations,
such as extrude. In this case you would set your UDO class to allow selection
of the owned object.
Even if UF_UDOBJ_ALLOW_SELECTION is set, the owned object is not eligible
to be selected interactively for deletion.
Environment : Internal and External
See Also:
History: Originally released in V16.0.2
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_set_owned_object_selection
(
UF_UDOBJ_class_t class_id, /* <I>
The class of the UDO which is being set.
*/
UF_UDOBJ_owned_object_selection_t value /* <I>
The selection type that is to be
set for this UDO class.
*/
);
/*****************************************************************************
Set the behavior of querying the class id given the class name. The default
mode is UF_UDOBJ_DONT_ALLOW_QUERY_CLASS_ID. This means that if you call
UF_UDOBJ_ask_class_id_of_name with the UDO's class name, an error code will be
returned, and the class id returned will be 0. This mechanism is used to
help protect the integrity of a proprietary UDO.
Setting the query to UF_UDOBJ_ALLOW_QUERY_CLASS_ID means that given a class name,
you can find the class id. This mechanism is used to pass the class id
across multiple shared libraries.
Environment : Internal and External
See Also:
History: Originally released in V16.0.2
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_set_query_class_id
(
UF_UDOBJ_class_t class_id, /* <I>
The class of the UDO which is being set.
*/
UF_UDOBJ_query_class_id_t value /* <I>
The query type that is to be
set for this UDO class.
*/
);
/*****************************************************************************
Set the behavior of warning the user if a UDO of the given class is found
in a part, but the code implementing the methods for the UDO is not loaded.
The default action is to not warn the user. If the UDO author sets this flag
to TRUE, all UDO's of this class that are created will be marked so that the
user will be warned if the UDO methods have not been loaded, but a UDO of the
class is in the part. This warning will be issued to the listing window,
when the first object of the given class is retrieved. This warning will
only be given once per session.
This flag is set on every UDO object. Therefore for any part,
there may be a mixture UDO objects of a given class, some having this flag
set to TRUE and some objects having the flag set to FALSE. This is
particularly true since all UDO objects created before NX 3.0 will have this
flag set to FALSE. If the UDO methods for a class are not loaded, any one
UDO with this flag set to TRUE in a part is enough for the warning to be
issued to the listing window.
Environment : Internal and External
See Also:
History: Originally released in NX 3.0
*****************************************************************************/
extern UFUNEXPORT int UF_UDOBJ_set_user_warn_flag
(
UF_UDOBJ_class_t class_id, /* <I>
The class of the UDO which is being set.
*/
logical value /* <I>
Should the user be warned if the UDO
methods are not loaded?
TRUE - the user will be warned
FALSE - the user will not be warned.
Note that the default if this routine is not
called is FALSE.
*/
);
#undef EXPORTLIBRARY
#endif /* UF_UDOBJ_H_INCLUDED */