the link type to create; any of these possibilities:
Link type 1 -- if the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected; if the UDO is updated the associated object is unaffected; if the associated object is deleted the UDO is also deleted; if the associated object is updated the UDO is updated
Link type 2 -- if the UDO is deleted the link between the UDO and the associated object is removed and the object is deleted; if the UDO is updated the associated NX object is unaffected; if the associated object is deleted, it is left in the data model in a condemned state and remains attached to the UDO; if the associated object is updated the UDO is unaffected
Link type 3 -- if the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected; if the UDO is updated the associated object is unaffected; if the associated object is deleted the link to the UDO is removed and the UDO is updated; if the associated object is updated the UDO is updated
Link type 4 -- if the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected; if the UDO is updated the associated object is unaffected; if the associated object is deleted the link to the UDO is removed and the UDO is unaffected; if the associated object is updated the UDO is unaffected
In most cases this will be the NX tag to associate the UDO with. However for the routine UF_UDOBJ_ask_udo_links_to_obj, this will return the tag of the UDO that the object is linked to.
object_status
unsigned int
the up-to-date indicator for the object associated with the UDO 0 = Up to date 1 = Out of date
these possibilities:
Link type 1 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
UDO is also deleted; if the
associated object is updated the
UDO is updated
Link type 2 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is deleted; if the
UDO is updated the associated NX
object is unaffected; if the
associated object is deleted, it
is left in the data model in a
condemned state and remains
attached to the UDO; if the
associated object is updated
the UDO is unaffected
Link type 3 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
link to the UDO is removed and
the UDO is updated; if the
associated object is updated the
UDO is updated
Link type 4 --
if the UDO is deleted the link
between the UDO and the
associated object is removed and
the object is unaffected; if the
UDO is updated the associated
object is unaffected; if the
associated object is deleted the
link to the UDO is removed and
the UDO is unaffected; if the
associated object is updated the
UDO is unaffected