UF_ROUTE_duct_reinforcement_parameters_s (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_reinforcement_params_t
- UF_ROUTE_duct_reinforcement_params_p_t
Overview
The duct reinforcement plugin evaluates the parent duct selected and determines
the various parameters for duct reinforceemnt creation. These parameters are
stored using the following struct.
Data Members
reinforcementType
parallelStockBlockVisibility
parallelStock
numberOfPairs
int
spacing
double
perpendicularStockBlockVisibility
reinforcementTypeBlockVisibility
perpendicularStock
interval
double
clearnce
double
editMode