UF_ROUTE_bend_radius_method_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_bend_radius_method_t
- UF_ROUTE_bend_radius_method_p_t
Overview
Bend corner creation methods.
Data Members
UF_ROUTE_bend_radius_method_radius
UF_ROUTE_bend_radius_method_ratio_to_diameter
UF_ROUTE_bend_radius_method_bend_radius_table
UF_ROUTE_bend_radius_method_inner_radius
UF_ROUTE_branch_path_numbering_sequence_method_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_branch_path_numbering_sequence_method_t
- UF_ROUTE_branch_path_numbering_sequence_method_p_t
Overview
Used by the Branch Path Numbering plugin.
See UFD_Routing_BranchPathNumbering.cxx for an example plugin.
Data Members
UF_ROUTE_branch_path_numbering_sequence_numbers
UF_ROUTE_branch_path_numbering_sequence_upper_case
UF_ROUTE_branch_path_numbering_sequence_lower_case
UF_ROUTE_duct_calculator_errors_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_calculator_errors_t
- UF_ROUTE_duct_calculator_errors_p_t
Overview
The duct size calculator plugins use this enumeration to tell the duct size calculator
dialog about any errors that may occur in a plugin.
Data Members
UF_ROUTE_DUCT_ERROR_OK = 0
UF_ROUTE_DUCT_NO_PLUGIN_FOUND
UF_ROUTE_DUCT_CANT_CALCULATE
UF_ROUTE_duct_parameter_types_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_parameter_types_t
- UF_ROUTE_duct_parameter_types_p_t
Overview
The duct size calculator dialog uses this enumeration to tell the plugin which parameter the dialog
is sending to the plugin. The plugin should then calculate the value for this parameter.
Data Members
UF_ROUTE_DUCT_HEIGHT
UF_ROUTE_DUCT_WIDTH
UF_ROUTE_DUCT_ASPECTRATIO
UF_ROUTE_DUCT_EQUIVALENT_DIAMETER
UF_ROUTE_DUCT_DIAMETER
UF_ROUTE_DUCT_AREA
UF_ROUTE_DUCT_VELOCITY
UF_ROUTE_DUCT_VOLFLOWRATE
UF_ROUTE_DUCT_SHAPE_CHANGE
UF_ROUTE_DUCT_DEFAULT
UF_ROUTE_duct_reinforcement_types_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_reinforcement_types_t
- UF_ROUTE_duct_reinforcement_types_p_t
Overview
The plugin for Duct Reinforcement uses this enumeration to tell the dialog
the type of reinforcement to create
Data Members
UF_ROUTE_DUCT_REINFORCEMENT_TYPE_NONE
UF_ROUTE_DUCT_REINFORCEMENT_TYPE_INSIDE
UF_ROUTE_DUCT_REINFORCEMENT_TYPE_OUTSIDE
UF_ROUTE_duct_segment_attribute_status_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_segment_attribute_status_t
- UF_ROUTE_duct_segment_attribute_status_p_t
Overview
The duct size calculator plugins use this enumeration to tell the duct size calculator
dialog about the attributes on the selected segments.
Data Members
UF_ROUTE_DUCT_EMPTY_ATTRIBUTES
UF_ROUTE_DUCT_ATTRIBUTES_NOT_EQUAL
UF_ROUTE_DUCT_VALID_ATTRIBUTES
UF_ROUTE_duct_shape_e (view source)
Defined in: uf_route.h
Also known as:
- UF_ROUTE_duct_shape_t
- UF_ROUTE_duct_shape_p_t
Overview
The duct size calculator dialog use this enumeration to tell the duct size calculator
plugin the shape of the duct being calculated.
Data Members
UF_ROUTE_DUCT_RECTANGULAR
UF_ROUTE_DUCT_CIRCULAR
UF_ROUTE_DUCT_FLATOVAL