UF_DPUD_ask_dpud (view source)
Defined in: uf_dpud.h
Overview
Return the UF_DPUD_id_t identifier which corresponds to the UF_CAM_exit_id_t
that was passed to the User Exit from NX.
Environment
Internal and External
int UF_DPUD_ask_dpud
(
UF_CAM_exit_id_t exit_id,
UF_DPUD_id_t * dpud_id
)
UF_DPUD_ask_drpos0 (view source)
Defined in: uf_dpud.h
Overview
Returns the identifier of the requested drive position of this request.
This drive position is available only when the purpose of the request is
UF_DPUD_GET_NEXT or UF_DPUD_GET_INTERMEDIATE.
Environment
Internal and External
int UF_DPUD_ask_drpos0
(
UF_DPUD_id_t dpud,
UF_DRPOS_id_t * drpos
)
UF_DPUD_ask_drpos1 (view source)
Defined in: uf_dpud.h
Overview
Return the identifier of the first input drive position of this request.
This drive position is available only when the purpose of the request is
UF_DPUD_GET_INTERMEDIATE.
Environment
Internal and External
int UF_DPUD_ask_drpos1
(
UF_DPUD_id_t dpud,
UF_DRPOS_id_t * drpos
)
UF_DPUD_ask_drpos2 (view source)
Defined in: uf_dpud.h
Overview
Return the identifier of the second input drive position of this request.
This drive position is available only when the purpose of the request is
UF_DPUD_GET_INTERMEDIATE.
Environment
Internal and External
int UF_DPUD_ask_drpos2
(
UF_DPUD_id_t dpud,
UF_DRPOS_id_t * drpos
)
UF_DPUD_ask_oper (view source)
Defined in: uf_dpud.h
Overview
Return the identifier for the operation requesting the service.
Environment
Internal and External
int UF_DPUD_ask_oper
(
UF_DPUD_id_t dpud,
UF_OPER_id_t * oper
)
UF_DPUD_ask_proj_option (view source)
Defined in: uf_dpud.h
Overview
Determine the projection vector option chosen by the user in the NX
dialog.
Environment
Internal and External
int UF_DPUD_ask_proj_option
(
UF_DPUD_id_t dpud,
UF_DPUD_proj_option_t * proj_option
)
UF_DPUD_ask_proj_vec (view source)
Defined in: uf_dpud.h
Overview
Determine the projection vector chosen by the user in the NX dialog,
if the projection vector option is UF_DPUD_proj_constant. For other
options the result of this call is undetermined.
Since the drive position projection vector in this case is automatically
set by the NX processor, there is no need to do it in the Open C
API program. This function is included only for the information it
provides.
Environment
Internal and External
int UF_DPUD_ask_proj_vec
(
UF_DPUD_id_t dpud,
double proj_vec [ 3 ]
)
UF_DPUD_id_t | dpud | Input | Identifier for a DPUD object |
double | proj_vec [ 3 ] | Output | The constant projection vector |
UF_DPUD_ask_purpose (view source)
Defined in: uf_dpud.h
Overview
Return the purpose of this request.
Environment
Internal and External
int UF_DPUD_ask_purpose
(
UF_DPUD_id_t dpud,
UF_DPUD_purpose_t * purpose
)
UF_DPUD_ask_ratio (view source)
Defined in: uf_dpud.h
Overview
Returns the ratio at which an intermediate drive position must be
generated. The value of this ratio is between 0.0 and 1.0. If ratio=
0.0, the Open C API program must return a copy of drpos2. Note:
while the parameterization of the drive path (used to associate the
ratio with a drive position) is not expected to equal the actual curve
length, it must be strictly monotonous and a continuous function of
the curve length.
This function is only available when the purpose of the request is
UF_DPUD_GET_INTERMEDIATE.
Environment
Internal and External
int UF_DPUD_ask_ratio
(
UF_DPUD_id_t dpud,
double* ratio
)
UF_DPUD_id_t | dpud | Input | Identifier for a DPUD object |
double* | ratio | Output | The ratio for the intermediate point |
UF_DPUD_ask_taxis_option (view source)
Defined in: uf_dpud.h
Overview
Determine the tool axis option chosen by the user in the NX dialog.
Environment
Internal and External
int UF_DPUD_ask_taxis_option
(
UF_DPUD_id_t dpud,
UF_DPUD_taxis_option_t * taxis_option
)
UF_DPUD_ask_tool_axis (view source)
Defined in: uf_dpud.h
Overview
Determine the tool axis chosen by the user in the NX dialog, if the
tool axis option is UF_DPUD_taxis_constant. For other options the
result of this call is undetermined.
Since the drive position tool axis in this case is automatically set by
the NX processor, there is no need to do it in the Open C API
program. This function is included only for the information it
provides.
Environment
Internal and External
int UF_DPUD_ask_tool_axis
(
UF_DPUD_id_t dpud,
double tool_axis [ 3 ]
)
UF_DPUD_id_t | dpud | Input | Identifier for a DPUD object |
double | tool_axis [ 3 ] | Output | The constant tool axis |
UF_DPUD_set_user_data_size (view source)
Defined in: uf_dpud.h
Overview
Set the size of the user data portion to be used for all drive postions.
This function is available only when the purpose of the request is
UF_DPUD_GET_USER_DATA_SIZE.
Environment
Internal and External
int UF_DPUD_set_user_data_size
(
UF_DPUD_id_t dpud,
int size
)
UF_DPUD_id_t | dpud | Input | Identifier for a DPUD object |
int | size | Input | Size of User data drive positions (bytes) |