/*
uf_oper_spec.h
File Description:
This file contains the documentation required for using the Open API
Interface to the pre-v16 Oper module.
******************************************************************************/
#ifndef UF_OPER__SPEC_H
#define UF_OPER__SPEC_H
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cam.h>
#include <uf_path.h>
#include <uf_oper_spec.h>
#include <libufun_cam_exports.h>
/***************************************************************************
***************************************************************************/
#define ERROR_UF_OPER_base 1360000
/********************************** Defines ***********************************/
#define UF_OPER_OPNAME_NCHARS 133
#define UF_OPER_OPNAME_BUFSIZE NX_BUFSIZE(UF_OPER_OPNAME_NCHARS)
/* */
#define UF_OPER_OPNAME_LEN (UF_OPER_OPNAME_BUFSIZE-1)
/* */
#define ERROR_UF_OPER_WRONG_OPER_TY (ERROR_UF_OPER_base + 1)
#define ERROR_UF_OPER_NOT_IMPLEMENTED (ERROR_UF_OPER_base + 2)
#define ERROR_UF_OPER_INVALID_PARAMETER (ERROR_UF_OPER_base + 3)
/****************************************************************************
NOTE :
An operation identifier of the type UF_OPER_id_t has to be used as the
input for all functions querying an operation
*****************************************************************************/
/********************************* Typedefs *********************************/
/* UF_OPER_id_t is the identifier for referring to a UF_OPER */
typedef void *UF_OPER_id_t;
/******************************* Prototypes **********************************/
/*****************************************************************************
Returns the UF_oper_id_t that corresponds to the UF_CAM_exit_id_t passed to the
User Exit from NX.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_oper(
UF_CAM_exit_id_t exit_id ,/* <I>
exit_id passed to user exit from NX
*/
UF_OPER_id_t * oper_id /* <O>
Operation Identifier
*/
);
/*****************************************************************************
This function copies the Operation name associated with "oper_id" to the memory
pointed at "op_name". This memory must be the same as UF_OPER_OPNAME_BUFSIZE bytes.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_name(
UF_OPER_id_t oper_id ,/* <I>
Operation identifier
*/
char op_name[UF_OPER_OPNAME_BUFSIZE] /* <O>
Pointer to at least UF_OPER_OPNAME_BUFSIZE bytes
*/
);
/*****************************************************************************
Returns the path identifier associated with "oper_id".
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_path(
UF_OPER_id_t oper_id ,/* <I>
Operation identifier
*/
UF_PATH_id_t * path_id /* <O>
Path identifier of this oper's path
*/
);
#undef EXPORTLIBRARY
#endif /* UF_OPER_SPEC_INCLUDED */