uc4500 (view source)
Defined in: uf_cfi.h
Overview
Open a file for binary buffered I/O. The open mode
is used to indicate how the file is to be accessed.
The file format is used both to specify a default extension to use and
for the write modes, the type to be stored in the file's header. For the
read mode, a format of zero may be specified indicating no default
extension.
A native operating system file may be opened by using the
appropriate file type. For example, a format of 4 opens a text file in
the native file system.
A successful open returns a simple integer channel number. This
channel number is to be passed to the routines for reading, writing,
skipping, and closing the file.
uc4510 (read characters), uc4511 (read integers), uc4512 (read reals),
and uc4513 (read bytes) are used to read primitive data types from a
file open with uc4500. Combinations of these types may be used to
create more complex data types. The I/O channel number returned by uc4500
is passed to these other routines.
uc4520 (write characters), uc4521 (write integers), uc4522 (write
reals), and uc4523 (write bytes) are used to write primitive data types
to a file opened with uc4500. Combinations of these calls are used to
create more complex types. The I/O channel number returned by uc4500
is passed to these other routines.
uc4530 (skip characters), uc4531 (skip integers), uc4532 (skip reals),
and uc4533 (skip bytes) are used to bypass primitive data types in a
file opened with uc4500. A combination of these may be used to skip
over more complex types. Skips may be backward by using negative
skip counts.
For characters, the count will be rounded up to the next integer
boundary (e.g. a write/read/skip of 5 will actually write/read/skip 8
characters).
Return
Return code:
<0 = error
>= 0 = i/o channel number
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4500
(
const char * fspec,
int omode,
int ftype
)
const char * | fspec | Input | File To Open |
int | omode | Input | Open Mode 1 = Read 2 = Write 3 = Write, Replace 5 = Update 7 = Scratch |
int | ftype | Input | File Format |
uc4504 (view source)
Defined in: uf_cfi.h
Overview
Open a text file for I/O. Only the routines uc4514,
uc4524, and uc4525 for reading and writing lines may be used on text
file. See the description of uc4500 for a description of the parameters.
For omode = 4, the file must exist and will be opened for write. The
file pointer will be initially positioned at the end of file.
For omode = 6, a printer is opened. If the filespec is blank, the
default printer will be opened.
Return
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4504
(
const char * fspec,
int omode,
int ftype
)
const char * | fspec | Input | File To Open |
int | omode | Input | Open Mode 1 = Read 2 = Write 3 = Write, Replace 4 = Append 6 = Printer |
int | ftype | Input | File Type |
uc4506 (view source)
Defined in: uf_cfi.h
Overview
Open a binary file for block I/O. Only the routines
uc4516 and uc4526 for reading and writing blocks may be used on a
file opened with uc4506. See the description of uc4500 for a
description of the parameters.
Return
Return code:
> 0 = error
<= 0 = I/O Channel Number
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4506
(
const char * fspec,
int omode,
int ftype
)
const char * | fspec | Input | File To Open |
int | omode | Input | Open Mode 1 = Read 2 = Write 3 = Write, Replace 5 = Update 7 = Scratch |
int | ftype | Input | File Type |
uc4507 (view source)
Defined in: uf_cfi.h
Overview
Open a file for record oriented I/O. Only the
routines uc4517 and uc4527 may be used to read and write records.
Record I/O is generally only supported for native files.
Return
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4507
(
const char * fspec,
int omode,
int ftype,
int rectype
)
const char * | fspec | Input | File Specification |
int | omode | Input | Open Mode 1 = Read 2 = Write 3 = Replace 5 = Update 7 = Scratch |
int | ftype | Input | File Type |
int | rectype | Input | Record Format = 0 = Variable Length Records > 0 = Fixed Record Length |
uc4508 (view source)
Defined in: uf_cfi.h
Overview
Open a directory for reading. Directory entries are read
using uc4518 with the fields picked out using uc4600 to uc4609.
Sub-directories may be opened using uc4509.
The dmode bit-mask is used to indicate the intention of the
application in using the directory. Bits zero through seven indicate
which fields from the file header to read and bits ten through thirteen
specify special directory options.
You can specify which bits to set by using the left shift operator in
conjuction with the bit wise or. For example, to set bits 11 and 13, you
would use the following declaration:
int dmode = (1 << 11) | (1 << 13);
A wildcard template may be used and is specified when the directory
is opened. It may be passed separate from the directory filespec or as
part of the directory filespec. For example:
dmode(bit 11) = 1, fspec = "disk/manager", wcard = ".prt" will
return out all parts in the manager's directory.
If neither dmode(bit 11) or dmode(bit 12) is set then all files will be
returned. dmode(bit 11) and dmode(bit 12) should not be
set at the same time.
If dmode(bit 13) is set then the caller is only interested in the names
of the files and none of the header attributes. If this is set then none
of the parameter dmode(bit 0) through dmode(bit 7) should be set.
If dmode(bit 10) is set then the caller is intending to open
sub-directories. If it is not set then uc4509 should not be called.
Return
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4508
(
const char * fspec,
int dmode,
int ftype,
const char * wcard
)
const char * | fspec | Input | Directory Specification |
int | dmode | Input | Bit-mask Of Open Options bit 0 = Read Owner Field 0 = No 1 = Yes bit 1 = Read Protection Classfield 0 = No 1 = Yes bit 2 = Read Status Field 0 = No 1 = Yes bit 3 = Read Length Field 0 = No 1 = Yes bit 4 = Read Dates 0 = No 1 = Yes bit 5 = Read Description Field 0 = No 1 = Yes bit 6 = Read Customer Area Field 0 = No 1 = Yes bit 7 = Read Machine Field 0 = No 1 = Yes bit 8-9 = Reserved bit 10 = Enable Sub-trees 0 = No 1 = Yes bit 11 = Template Given 0 = No 1 = Yes, Template In wcard bit 12 = Directory Contains Wildcards 0 = No 1 = Yes bit 13 = Read Filenames Only 0 = No 1 = Yes bit 14-15 = Reserved |
int | ftype | Input | This argument is no longer used. |
const char * | wcard | Input | Wildcard Template |
uc4509 (view source)
Defined in: uf_cfi.h
Overview
Open a subdirectory of the currently open directory.
The previous directory entry read by uc4518 must have been of type
directory (format 100-112) otherwise the error 'not a directory'
is returned. Subdirectories are closed using uc4549.
Environment
Internal and External
See Also
Required License(s)
gateway
uc4510 (view source)
Defined in: uf_cfi.h
Overview
Read characters from a file opened with uc4500.
For characters, the count will be rounded up to the next integer
boundary (e.g. a read of 5 will actually read 8 characters).
Integer variables are used for storing the characters in byte format.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4510
(
int chan,
int len,
char cbuf [ UF_MAXWORD ]
)
int | chan | Input | I/O Channel Number returned from uc4500. |
int | len | Input | Number Of Characters To Read |
char | cbuf [ UF_MAXWORD ] | Output | Array To Read Characters Into |
uc4511 (view source)
Defined in: uf_cfi.h
Overview
Read integers from a file opened with uc4500.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4511
(
int chan,
int len,
int * sibuff
)
int | chan | Input | I/O Channel Number returned from uc4500. |
int | len | Input | Number Of Integers To Read |
int * | sibuff | Output | Array To Read Integers Into |
uc4512 (view source)
Defined in: uf_cfi.h
Overview
Read reals from a file opened with uc4500.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4512
(
int chan,
int len,
double rbuff [ ]
)
int | chan | Input | I/O Channel Number returned from uc4500 |
int | len | Input | Number Of Reals To Read |
double | rbuff [ ] | Output | Array To Read Reals Into |
uc4513 (view source)
Defined in: uf_cfi.h
Overview
Read bytes from a file opened with uc4500.
Environment
Internal and External
Required License(s)
gateway
int uc4513
(
int chan,
int len,
char bbuf [ UF_MAXWORD ]
)
int | chan | Input | I/O Channel Number returned by uc4500 |
int | len | Input | Number Of Bytes To Read |
char | bbuf [ UF_MAXWORD ] | Output | Array To Read Bytes Into |
uc4514a (view source)
Defined in: uf_cfi.h
Overview
Read a line of text from a file opened with uc4504.
Return
Return code
< 0 = Error
>= 0 = Length Of Line Read
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4514a
(
int chan,
char * * cbuf
)
int | chan | Input | I/O channel number returned by uc4504 |
char * * | cbuf | Output to UF_*free* | Line read. The buffer must be freed with UF_free() |
uc4516 (view source)
Defined in: uf_cfi.h
Overview
Randomly read blocks from a file opened with
uc4506. Data is always read on a block boundary.
Return
Return code
< 0 = Error
> 0 = Number of bytes actually read
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4516
(
int chan,
int block,
int bytes,
char * cbuf
)
int | chan | Input | I/O channel number returned by uc4506 |
int | block | Input | Starting block number to read (from 0) |
int | bytes | Input | Number of bytes to read |
char * | cbuf | Output | Data read |
uc4517 (view source)
Defined in: uf_cfi.h
Overview
Read the next record from a file opened using uc4507.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4517
(
int chan,
int * bytes,
char * cbuf
)
int | chan | Input | I/O channel number returned by uc4507 |
int * | bytes | Output | Length of record read in bytes |
char * | cbuf | Output | Array to read record into |
uc4518 (view source)
Defined in: uf_cfi.h
Overview
Read the next directory entry and save the entry's
information in memory. This information may then be accessed by the
routines uc4600 through uc4609.
Return
Return code
< 0 = Error
0 = Entry Read
1 = End Of Subdirectory
2 = End Of Directory
Environment
Internal and External
See Also
Required License(s)
gateway
uc4519 (view source)
Defined in: uf_cfi.h
Overview
Returns the full filespec of the last directory entry
read. This is provided so the Open C API program need not be
concerned with the syntax of filespecs in forming them.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4519
(
char fspec [ MAX_FSPEC_BUFSIZE ]
)
char | fspec [ MAX_FSPEC_BUFSIZE ] | Output | Full file specification of the last directory entry read. |
uc4520 (view source)
Defined in: uf_cfi.h
Overview
Write characters to a file opened with uc4500.
The count will be rounded up to the next integer
boundary (e.g. a write of 5 will actually write 8 characters).
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4520
(
int chan,
long len,
const char * cbuff
)
int | chan | Input | I/O channel number returned by uc4500. |
long | len | Input | Number of characters to write |
const char * | cbuff | Input | Character data to write |
uc4521 (view source)
Defined in: uf_cfi.h
Overview
Write integers to a file opened with uc4500.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4521
(
int chan,
long len,
int * sibuff
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of integers to write |
int * | sibuff | Input | Integer data to write |
uc4522 (view source)
Defined in: uf_cfi.h
Overview
Write reals to a file opened with uc4500.
Environment
Internal and External
Required License(s)
gateway
int uc4522
(
int chan,
long len,
double rbuff [ ]
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of reals to write |
double | rbuff [ ] | Input | Real data to write |
uc4523 (view source)
Defined in: uf_cfi.h
Overview
Write bytes to a file opened with uc4500.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4523
(
int chan,
long len,
const void * bbuff
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of bytes to write |
const void * | bbuff | Input | Byte data to write |
uc4524 (view source)
Defined in: uf_cfi.h
Overview
Write a line to a text file. Only complete lines may
be written to a text file. The addition of any delimiters (e.g. newline)
is done automatically.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4524
(
int chan,
const char * cbuf
)
int | chan | Input | I/O channel number returned by uc4504 |
const char * | cbuf | Input | Line to write |
uc4525 (view source)
Defined in: uf_cfi.h
Overview
uc4525 is used to write a page break to a text file.
Environment
Internal and External
See Also
Required License(s)
gateway
int | chan | Input | I/O channel number returned by uc4504 |
uc4526 (view source)
Defined in: uf_cfi.h
Overview
Randomly write to a file opened with uc4506. The
data is always written on a block boundary.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4526
(
int chan,
int block,
int bytes,
const char * buf
)
int | chan | Input | I/O channel number returned by uc4506 |
int | block | Input | Starting block number to write (from 0) |
int | bytes | Input | Number of bytes to write |
const char * | buf | Input | Data to write |
uc4527 (view source)
Defined in: uf_cfi.h
Overview
Write a record to a file opened with uc4507. For fixed
length record files, the parameter bytes is ignored.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4527
(
int chan,
int bytes,
const char * cbuf
)
int | chan | Input | I/O channel number returned by uc4507 |
int | bytes | Input | Length of record to write in bytes |
const char * | cbuf | Input | Buffer containing data to write |
uc4530 (view source)
Defined in: uf_cfi.h
Overview
Skip characters in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4530
(
int chan,
long len
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of characters to skip over |
uc4531 (view source)
Defined in: uf_cfi.h
Overview
Skip integers in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment
Internal and External
Required License(s)
gateway
int uc4531
(
int chan,
long len
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of integers to skip over |
uc4532 (view source)
Defined in: uf_cfi.h
Overview
Skip reals in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment
Internal and External
Required License(s)
gateway
int uc4532
(
int chan,
long len
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of reals to skip over |
uc4533 (view source)
Defined in: uf_cfi.h
Overview
Skip bytes in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment
Internal and External
Required License(s)
gateway
int uc4533
(
int chan,
long len
)
int | chan | Input | I/O channel number returned by uc4500 |
long | len | Input | Number of bytes to skip over |
uc4534 (view source)
Defined in: uf_cfi.h
Overview
Find the current position within a file opened with
uc4500. That position may then be restored using uc4535.
Return
Return code:
< 0 = Error
>= 0 = File position
Environment
Internal and External
See Also
Required License(s)
gateway
int | chan | Input | I/O channel number returned by uc4500 |
uc4535 (view source)
Defined in: uf_cfi.h
Overview
Restore the read/write position within a file
previously saved using uc4534. The file must have been opened with
uc4500.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4535
(
int chan,
long pos
)
int | chan | Input | I/O channel number returned by uc4500 |
long | pos | Input | File position returned by uc4534 |
uc4536 (view source)
Defined in: uf_cfi.h
Overview
Reposition a file back to the beginning. This may be
used for binary, text, and record I/O files.
Environment
Internal and External
Required License(s)
gateway
int | chan | Input | I/O channel number |
uc4540 (view source)
Defined in: uf_cfi.h
Overview
Close a file opened with either uc4500, uc4504,
uc4506, or uc4507. The close disposition is used to indicate whether a
file opened for write is to be saved or not. A normal close will make
the file permanent and delete any previous file with the same name.
An abort close will delete the file and retain any previous file with the
same name.
Environment
Internal and External
Required License(s)
gateway
int uc4540
(
int chan,
int disp
)
int | chan | Input | I/O channel number |
int | disp | Input | Disposition 0 = Normal close 1 = Abort close |
uc4544 (view source)
Defined in: uf_cfi.h
Overview
Determine characteristics of an open file given its I/O channel number.
The integer date/times in qreslt (if qreslt = 6) can be converted to
character strings using uc4582.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4544
(
int chan,
int qitem,
int * qreslt
)
int | chan | Input | I/O channel number |
int | qitem | Input | Item to inquire: 1 = File System 2 = File Type 3 = Last Error 4 = Record Format 5 = Maximum Record Size 6 = Creation, Modify, Access Dates |
int * | qreslt | Output | Query result: For qreslt = 1, 2 = NATIVE For qreslt = 2, See File Types For qreslt = 3, Last read or write error For qreslt = 4, = 0 = Variable length records > 0 = Fixed record length For qreslt = 5, Maximum record/line length For qreslt = 6, qreslt is an array of 6 integers (0)-(1) = Creation Date,Time (2)-(3) = Modification Date,Time (4)-(5) = Last Access Date,Time |
uc4547 (view source)
Defined in: uf_cfi.h
Overview
Determines the file length (in bytes) of
an open file given its I/O channel number.
Environment
Internal and External
Required License(s)
gateway
int uc4547
(
int chan,
int qitem,
int * qreslt
)
int | chan | Input | I/O channel number |
int | qitem | Input | Item to query 1 = File length in bytes |
int * | qreslt | Output | Query result |
uc4548 (view source)
Defined in: uf_cfi.h
Overview
Close any directories opened with uc4508. If any
subdirectories are open, they will be closed as well.
Environment
Internal and External
See Also
Required License(s)
gateway
uc4549 (view source)
Defined in: uf_cfi.h
Overview
Close a subdirectory opened with uc4509. Directory
reads will then continue with the previous directory.
Environment
Internal and External
See Also
Required License(s)
gateway
uc4560 (view source)
Defined in: uf_cfi.h
Overview
Checks whether the specified file of the given type exists.
NOTE: Mixed or upper case file names may not be found if the
environment variable UGII_OPTION = LOWER is set.
Passing an ftype of 0 will look for a file but does not work for a directory.
To check for a directory the ftype must be set to 100.
Return
Return code:
< 0 = Error
= 0 = File Exists
= 1 = File Does Not Exist
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4560
(
const char * fspec,
int ftype
)
const char * | fspec | Input | File to check |
int | ftype | Input | File type 0 will check for files 100 will check for directories |
uc4561 (view source)
Defined in: uf_cfi.h
Overview
Remove a given file from the file system.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4561
(
const char * fspec,
int ftype
)
const char * | fspec | Input | File to delete |
int | ftype | Input | File type |
uc4562 (view source)
Defined in: uf_cfi.h
Overview
Change the name of a given file. The new file name
should be a simple name (e.g. no directory specification).
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4562
(
const char * fspec,
int ftype,
const char * fspec2
)
const char * | fspec | Input | Old file name |
int | ftype | Input | File type |
const char * | fspec2 | Input | New file name |
uc4563 (view source)
Defined in: uf_cfi.h
Overview
Create an empty directory.
Environment
Internal and External
Required License(s)
gateway
int uc4563
(
const char * fspec,
int ftype
)
const char * | fspec | Input | Directory to create |
int | ftype | Input | File type |
uc4564 (view source)
Defined in: uf_cfi.h
Overview
Retrieve the header information of a single file and
store it in memory. The information may then be retrieved using
uc4600 through uc4609.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4564
(
const char * fspec,
int ftype,
int fmode
)
const char * | fspec | Input | File specification from which to read header |
int | ftype | Input | File type |
int | fmode | Input | Bit-mask Specifying Header Fileds Desired bit 0 = Read Owner Field 0 = No 1 = Yes bit 1 = Read Protection Class Field 0 = No 1 = Yes bit 2 = Read Status Field 0 = No 1 = Yes bit 3 = Read Length Field 0 = No 1 = Yes bit 4 = Read Dates 0 = No 1 = Yes bit 5 = Read Description Field 0 = No 1 = Yes bit 6 = Read Customer Area Field 0 = No 1 = Yes bit 7 = Read Machine Field 0 = No 1 =yes bit 8-15 = Reserved |
uc4565 (view source)
Defined in: uf_cfi.h
Overview
Read the current default value for a directory.
Environment
Internal and External
Required License(s)
gateway
int uc4565
(
int def,
char fspec [ MAX_FSPEC_BUFSIZE ]
)
int | def | Input | Default to read: 1 = Current directory 2 = '$' directory 3 = '!' directory |
char | fspec [ MAX_FSPEC_BUFSIZE ] | Output | Current Setting |
uc4566 (view source)
Defined in: uf_cfi.h
Overview
Change the current user's directory.
Environment
Internal and External
Required License(s)
gateway
int uc4566
(
int def,
const char * fspec
)
int | def | Input | Default to change: 1 = Current directory 2 = '$' directory 3 = '!' directory |
const char * | fspec | Input | New default value |
uc4567 (view source)
Defined in: uf_cfi.h
Overview
Copies or moves a file from a source file specification to a destination file
specification. When any move option is used, the source file will only be
deleted after it has been successfully copied to the destination file.
Using a file type of -1 indicates "any file type" so changing extensions
during the copy or move operation will work correctly.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4567
(
const char * srcspc,
const char * dstspc,
int cmode,
int stype,
int dtype
)
const char * | srcspc | Input | Source file specification |
const char * | dstspc | Input | Destination file specification |
int | cmode | Input | Specifies Copy/Move Options: = UF_CFI_COPY_NEVER_REPLACE = UF_CFI_COPY_ALWAYS_REPLACE = UF_CFI_COPY_REPLACE_IF_NEWER = UF_CFI_COPY_LEGACY (same as UF_CFI_COPY_NEVER_REPLACE) = UF_CFI_MOVE_NEVER_REPLACE = UF_CFI_MOVE_ALWAYS_REPLACE = UF_CFI_MOVE_REPLACE_IF_NEWER = UF_CFI_MOVE_LEGACY (same as UF_CFI_MOVE_NEVER_REPLACE) |
int | stype | Input | Source file type |
int | dtype | Input | Destination file type |
uc4570 (view source)
Defined in: uf_cfi.h
Overview
Examine a filespec and make sure it conforms to the syntax of the file
system.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4570
(
const char * fspec,
int ftype
)
const char * | fspec | Input | File specification to validate |
int | ftype | Input | File type |
uc4571 (view source)
Defined in: uf_cfi.h
Overview
Examine a filespec and make sure it is a valid directory specification for
the file system. A "directory file spec" is a path to a file which is a
directory.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4571
(
const char * fspec,
int ftype
)
const char * | fspec | Input | Directory File Specification To Validate |
int | ftype | Input | File Type |
uc4572 (view source)
Defined in: uf_cfi.h
Overview
Examine a filespec and make sure it is a valid wildcard directory specification
for the file system. This will also indicate whether there were any
wildcard characters in the filespec. To find all files that match the wildcard
filespec, open the directory with uc4508 and supply the wildcard filespec,
then read (uc4518) each matching entry and the corresponding filespec (uc4519).
Return
Return code:
= 0 = Valid file specification
= 1 = Valid with wildcards
Anything else is an error
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4572
(
const char * fspec,
int ftype
)
const char * | fspec | Input | File specification to validate |
int | ftype | Input | File type |
uc4573 (view source)
Defined in: uf_cfi.h
Overview
Given a filespec return its fully qualified equivalent. If
a non-zero file type is given, the extension will also be set. For
example, the native system with a default directory DISK2/JOE
fspec = "foo", type = 2 will produce expfspec = "DISK2/JOE/FOO.PRT"
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4573
(
const char * fspec,
int ftype,
char expfspec [ MAX_FSPEC_BUFSIZE ]
)
const char * | fspec | Input | File specification to expand |
int | ftype | Input | File type |
char | expfspec [ MAX_FSPEC_BUFSIZE ] | Output | Expanded file specification |
uc4574 (view source)
Defined in: uf_cfi.h
Overview
Accept a filespec and removes any directory path, extension,
and any system specific information and returns the resultant simple
filename. For example:
fspec = "/DISK1/JOE/FOO.PRT", ftype = 2 will produce fname = "FOO".
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4574
(
const char * fspec,
int ftype,
char fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ]
)
const char * | fspec | Input | File specification from which to extract name |
int | ftype | Input | File type |
char | fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ] | Output | Simple file name |
uc4575 (view source)
Defined in: uf_cfi.h
Overview
Combine a directory with a filename producing a file specification (filespec).
For example:
dspec = "/manager", ftype = 2, fname = "bar"
will produce fspec = "/MANAGER/BAR.PRT".
If the file name is a directory, using a filetype of 100 will merge the
directories. For example:
dspec = "/manager", ftype = 100, fname = "bar"
will produce fspec = "/MANAGER/BAR".
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4575
(
const char * dspec,
int ftype,
const char * fname,
char fspec [ MAX_FSPEC_BUFSIZE ]
)
const char * | dspec | Input | Directory |
int | ftype | Input | File type |
const char * | fname | Input | File name |
char | fspec [ MAX_FSPEC_BUFSIZE ] | Output | Resultant file specification |
uc4576 (view source)
Defined in: uf_cfi.h
Overview
Take a filespec and returns its directory and filename components. For example:
fspec = "/Manager/Work/BENCH", ftype = 2
Note that this routine is impacted by the UGII_OPTION environment variable,
so if UGII_OPTION=lower is set, then the above example will produce:
dspec = "/manager/work" and fname = "bench.prt".
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4576
(
const char * fspec,
int ftype,
char dspec [ MAX_FSPEC_BUFSIZE ] ,
char fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ]
)
const char * | fspec | Input | File specification to split up |
int | ftype | Input | File type |
char | dspec [ MAX_FSPEC_BUFSIZE ] | Output | Directory component |
char | fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ] | Output | File name component |
uc4577 (view source)
Defined in: uf_cfi.h
Overview
The name returned is a unique name for a temporary file. The resultant
filename is unique from other processes at the time. From a single
process, filenames will begin duplicating after the first 1,679,615 calls
to uc4577. Temporary files should be deleted when no longer needed by an
application. If the files are not deleted, there is a chance that the same
name may come up again if the same user happens to get the same process id
on a later date.
The maximum number of characters which will be returned is 12.
Environment
Internal and External
Required License(s)
gateway
int uc4577
(
char fname [ UF_MAX_UNIQUE_FILE_NAME_BUFSIZE ]
)
char | fname [ UF_MAX_UNIQUE_FILE_NAME_BUFSIZE ] | Output | Unique filename |
uc4578 (view source)
Defined in: uf_cfi.h
Overview
Remove the file extension from a given file specification and
returns the resultant file specification.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4578
(
const char * fspec,
int ftype,
char dspec [ MAX_FSPEC_BUFSIZE ]
)
const char * | fspec | Input | File specification |
int | ftype | Input | File type |
char | dspec [ MAX_FSPEC_BUFSIZE ] | Output | Resultant file specification |
uc4579 (view source)
Defined in: uf_cfi.h
Overview
Form the full filespec, given a simple name of a file
in the UGII_UTIL directory.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4579
(
const char * fname,
int ftype,
char fspec [ MAX_FSPEC_BUFSIZE ]
)
const char * | fname | Input | File name |
int | ftype | Input | File type |
char | fspec [ MAX_FSPEC_BUFSIZE ] | Output | Resultant file specification |
uc4580 (view source)
Defined in: uf_cfi.h
Overview
return the four character symbolic name for a given ftype
code (e.g.: 'PART' for ftype code 2). Many ftype codes will return
'TEXT' which indicates the file's contents may be displayed as ascii
data. Unnamed ftypes will have their numeric code returned in ascii.
Return
Return code:
< 0 = Error
= 0 = Format Returned
= 1 = Format Undefined
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4580
(
int ftype,
char symb [ 5 ]
)
int | ftype | Input | File type |
char | symb [ 5 ] | Output | Symbolic name |
uc4581 (view source)
Defined in: uf_cfi.h
Overview
Convert the symbolic character representation of a file type
into its numeric equivalent. For example, "PART" translates to a 2.
Return
Return code:
= 0 = Unknown Symbolic Name
> 0 = File Type
Environment
Internal and External
Required License(s)
gateway
int uc4581
(
const char * symb
)
const char * | symb | Input | Symbolic file type |
uc4582 (view source)
Defined in: uf_cfi.h
Overview
Convert NX computational time to display form. Two forms are available
for the date and two forms are available for the time.
A date or time of -1 returns the current date and/or time.
NOTE: In option 9 of the dtype argument, "formatted for the locale"
means that the date and time string is appropriate for the language in
which the user's operating system environment runs under.
Return
Return code:
0 = No error
not 0 = Error code
Environment
Internal and External
See Also
History
The dtype argument was modified in V13.0 to
increase the number of options from 4 to 9.
Required License(s)
gateway
int uc4582
(
int date [ 2 ] ,
int dtype,
char date_string [ 21 ] ,
char time [ 21 ]
)
int | date [ 2 ] | Input | Computational time: [0] Date [1] Time |
int | dtype | Input | Date And time representation: 1 = mm/dd/yy, hh:mm 2 = mm/dd/yy, hh:mm xM 3 = dd-mmm-yy, hh:mm 4 = dd-mmm-yy, hh:mm xM 5 = mm/dd/yyyy, hh:mm 6 = mm/dd/yyyy, hh:mm xM 7 = dd-mmm-yyyy, hh:mm 8 = dd-mmm-yyyy, hh:mm xM 9 = Formatted for the locale where 'mm' = numeric month, 'dd' = day, 'yy' = two digit year, 'yyyy' = four digit year, 'mmm' = symbolic month, 'hh' = hour, 'mm' = minute, 'x' = 'A' or 'P' When a blank is passed in for 'x', dtype = 8 will default to 12 hour time format where dtype = 7 will display a 24 hour time format. Note: On Windows any string can be specified as AM/PM by using Control Panel -> Regional and Language Options -> Customize -> Regional Options -> Time |
char | date_string [ 21 ] | Output | Date (20 characters max) |
char | time [ 21 ] | Output | Time (20 characters max) |
uc4583 (view source)
Defined in: uf_cfi.h
Overview
Convert a character date and time to NX computational date and time.
Return
Return Code:
0 = Success
1 = Failure
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4583
(
const char * date,
const char * time,
int* dandt
)
const char * | date | Input | Date in any of the following forms MM/DD/YY DD-MMM-YY DDMMMYY MM/DD/YYYY DD-MMM-YYYY DDMMMYYYY If date is blank, the current date is used |
const char * | time | Input | Time in either of the following forms HH:MM HH:MM xM (x = 'A' or 'P') If time is blank, the current time is used |
int* | dandt | Output | Date And Time (1) = Computational Date (2) = Computational Time |
uc4595 (view source)
Defined in: uf_cfi.h
Overview
Query the user name, String Result
Environment
Internal and External
Required License(s)
gateway
int uc4595
(
int qitem,
char str [ 17 ]
)
int | qitem | Input | Item to query: 1 = Username |
char | str [ 17 ] | Output | Query result. This must be a buffer big enough to hold the user name. |
uc4596 (view source)
Defined in: uf_cfi.h
Overview
Query a set of characteristics. The result for each item code follows:
Login Status: (qitem = 1)
bit 0 = Login Status
0 = NOT LOGGED IN
1 = LOGGED IN
bit 1 = Username Status
0 = DO NOT NEED A USERNAME TO LOGIN
1 = USERNAME NEEDED FOR LOGIN
bit 2 = Password Status
0 = DO NOT NEED A PASSWORD TO LOGIN
1 = PASSWORD NEEDED FOR LOGIN
bits 3-15 = Reserved
File Header Support: (qitem = 2)
bit 0 = Owner Supported
0 = NO
1 = YES
bit 1 = Protection Classes Supported
0 = NO
1 = YES
bit 2 = Status Word Supported
0 = NO
1 = YES
bit 3-4 = Reserved
bit 5 = Description Supported
0 = NO
1 = YES
bit 6 = Customer Area Supported
0 = NO
1 = YES
bit 7 = Non-Native Files Supported
0 = NO
1 = YES
bits 8-15 = Reserved
Environment
Internal and External
Required License(s)
gateway
int uc4596
(
int qitem,
int * qreslt
)
int | qitem | Input | Item to query 1 = Login status 2 = File header fields supported |
int * | qreslt | Output | Query result |
uc4599 (view source)
Defined in: uf_cfi.h
Overview
Translate an error code to the text associated with it.
Due to the way error handling is done in the file system routines, the
error text should be retrieved before another error occurs otherwise
the error message might be lost.
Environment
Internal and External
Required License(s)
gateway
int uc4599
(
int ug_errorno,
char errstg [ MAX_LINE_BUFSIZE ]
)
int | ug_errorno | Input | Error Code |
char | errstg [ MAX_LINE_BUFSIZE ] | Output | Error Text |
uc4600 (view source)
Defined in: uf_cfi.h
Overview
Return the simple file name of the last file read with uc4518 or uc4564..
To obtain the full file specification, including the directory use uc4519.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4600
(
char fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ]
)
char | fname [ UF_CFI_MAX_FILE_NAME_BUFSIZE ] | Output | Filename |
uc4601 (view source)
Defined in: uf_cfi.h
Overview
Return the file type of the last file read with uc4518 or uc4564..
You may use uc4581 to translate the file type to a character string.
Return
Return code:
< 0 = error
>= 0 = file type
Environment
Internal and External
See Also
Required License(s)
gateway
uc4602 (view source)
Defined in: uf_cfi.h
Overview
Return the status word of the last file read with uc4518 or uc4564..
Environment
Internal and External
See Also
Required License(s)
gateway
int * | fsts | Output | Status word |
uc4603 (view source)
Defined in: uf_cfi.h
Overview
Return the owner of the last file read with uc4518 or uc4564..
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4603
(
char owner [ 17 ]
)
char | owner [ 17 ] | Output | Owner of file (16 characters max) |
uc4605 (view source)
Defined in: uf_cfi.h
Overview
Return the length of the last file read with uc4518 or uc4564..
Return
Return code:
>= 0 = File Length In Bytes
< 0 = error code
Environment
Internal and External
See Also
Required License(s)
gateway
uc4606 (view source)
Defined in: uf_cfi.h
Overview
Return the creation, modification, and last access date/time
of the last file read with uc4518 or uc4564..
Use uc4582 to convert the date/time to character strings.
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4606
(
int * cdate,
int * mdate,
int * ldate
)
int * | cdate | Output | Two word array containing the creation date and time |
int * | mdate | Output | Two word array containing the modification date and time |
int * | ldate | Output | Two word array containing the last access date and time |
uc4607 (view source)
Defined in: uf_cfi.h
Overview
Return the descriptions area of the last file read with uc4518 or uc4564..
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4607
(
char darea [ MAX_LINE_BUFSIZE ]
)
char | darea [ MAX_LINE_BUFSIZE ] | Output | Description Area (132 characters max) |
uc4608 (view source)
Defined in: uf_cfi.h
Overview
Return the customer area of the last file read with uc4518 or uc4564..
Environment
Internal and External
See Also
Required License(s)
gateway
int uc4608
(
char carea [ MAX_LINE_BUFSIZE ]
)
char | carea [ MAX_LINE_BUFSIZE ] | Output | Customer area (132 characters max) |
uc4609 (view source)
Defined in: uf_cfi.h
Overview
Return the machine field of the last file read with uc4518 or uc4564.
These values are available for part files only. Parts filed in
V10.0 or earlier return unknown values.
Return
Return code:
< 0 = error
1 = APOLLO
2 = DEC VAX/VMS
3 = HP CISC
4 = HP RISC
5 = SUN 3
6 = SUN SPARC
7 = DEC RISC (ULTRIX)
8 = SGI
9 = DATA GENERAL
10 = IBM MVS
11 = IBM AIX
12 = AXP/OSF
13 = AXP/VMS
Environment
Internal and External
See Also
Required License(s)
gateway
uc4612 (view source)
Defined in: uf_cfi.h
Overview
Modify the status header field of a file. An error returns if the file
system does not support a status field or the user does not have the privilege
to change it.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4612
(
const char * fname,
int ftype,
int fsts
)
const char * | fname | Input | File name |
int | ftype | Input | File type |
int | fsts | Input | New status value |
uc4613 (view source)
Defined in: uf_cfi.h
Overview
Modify the owner header field of a file. An error returns if the file system
does not support an owner field or the user does not have the privilege to
change it (some operating systems may require root privilege to change file
ownership).
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4613
(
const char * fname,
int ftype,
const char * owner
)
const char * | fname | Input | File name to change the owner of |
int | ftype | Input | File type |
const char * | owner | Input | New owner value |
uc4617 (view source)
Defined in: uf_cfi.h
Overview
Change the description header field of a file. An
error is returned if the file system does not support a description field or
the user does not have the privilege to change it.
Environment
Internal and External
See Also
For description of file types see
table
Required License(s)
gateway
int uc4617
(
const char * fname,
int ftype,
const char * desc
)
const char * | fname | Input | File name to change description of |
int | ftype | Input | File type |
const char * | desc | Input | New description value |
uc4618 (view source)
Defined in: uf_cfi.h
Overview
Change the customer area header field of a file. An
error will be returned if the file system does not support a customer
area field or the user does not have the privilege to change it.
This function modifies the part file on disk and should not
be used on a part file that has already been opened in NX. If this
occurs, the part cannot be saved. Use UF_PART_set_customer_area to
modify the customer area of a loaded part.
Environment
Internal and External
See Also
UF_PART_set_customer_area
For description of file types see
table
Required License(s)
gateway
int uc4618
(
const char * fname,
int ftype,
const char * carea
)
const char * | fname | Input | File name to change the customers area of |
int | ftype | Input | File type |
const char * | carea | Input | New customer area value |
uc4620 (view source)
Defined in: uf_cfi.h
Overview
Read a switch from the program command line given the name of the switch.
All switches are global switches; they may appear anywhere on the command line.
Switches may have a value or no value. For example:
/LIST=FOO.LIS switch with a value
/LIST switch with no value
Switches must match completely. If sname is "USERNAME", you
must enter the full text string.
Under UNIX, switches take the form:
-name no value
-name=value switch with a value
Switches are separated by blanks on UNIX. For example:
ugraf -user=manager -pass=frogs
Under WNT, switches take the form:
-name no value
-name:value switch with a value
-name=value switch with a value
NOTE: Use uc4624 in conjunction with this function. You must call
uc4624 before calling either uc4620 or uc4621.
Return
Return code:
< 0 = Error
0 = Switch Not Present
1 = Switch Found With No Value
3 = Switch Found With A Value
Environment
External
See Also
Required License(s)
gateway
int uc4620
(
const char * sname,
char swstg [ MAX_LINE_BUFSIZE ]
)
const char * | sname | Input | Switch name |
char | swstg [ MAX_LINE_BUFSIZE ] | Output | Switch value |
uc4621 (view source)
Defined in: uf_cfi.h
Overview
Read arguments from the command line. Each argument may be read only once.
NOTE: Use uc4624 in conjunction with this function. You must call
uc4624 before calling either uc4620 or uc4621.
Return
Return code:
< 0 = Error
0 = Argument Not Present
1 = Argument Found
Environment
External
See Also
Required License(s)
gateway
int uc4621
(
char nxtarg [ MAX_FSPEC_BUFSIZE ]
)
char | nxtarg [ MAX_FSPEC_BUFSIZE ] | Output | Argument Value |
uc4622 (view source)
Defined in: uf_cfi.h
Overview
Returns an argument list to the GRIP xspawn command. The returned string
can not exceed 132 characters.
Environment
Internal and External
Required License(s)
gateway
char * | ip1 | Input | The return argument list |
uc4623 (view source)
Defined in: uf_cfi.h
Overview
Returns a pointer to a string which is the release number of the
specified part file. Some of the possible values are shown for the
description of cr2. You must allocate sufficient size for the relnum
array. For example, you could use MAX_FSPEC_BUFSIZE (prototyped in
uf_defs.h) for the size of the array.
Environment
Internal and External
Required License(s)
gateway
int uc4623
(
const char * fspec,
char relnum [ 133 ]
)
const char * | fspec | Input | Part file name |
char | relnum [ 133 ] | Output | Release number An example of possible Return Values are: V8, V9, V10, V10.1, V10.2, V10.3 etc. |
uc4624 (view source)
Defined in: uf_cfi.h
Overview
Save argument names for use with uc4620 and uc4621. The prog
parameter is not used. It is only present for backward compatibility.
You must use uc4624 before calling uc4620 or uc4621.
Note that uc4624 expects to receive the argc and argv values passed to the
program from main, and so the values in argv are assumed to be in the current
users locale not UTF8 data. As such this routine does not honor the setting of the text
mode made by calling UF_TEXT_set_text_mode().
Environment
External
See Also
Required License(s)
gateway
int uc4624
(
int prog,
int argc,
char * * argv
)
int | prog | Input | Not used |
int | argc | Input | Argument count |
char * * | argv | Input | array of argument names. This data is always assumed to be in the users current locale. |
uc4650 (view source)
Defined in: uf_cfi.h
Overview
Outputs a sorted directory listing to the Information Window if it has
been opened. Use UF_UI_open_listing_window to open the
Information Window. Dates in cbuf must be in the format
DD-MMM-YY (eg. 04-JUL-89).
Return
Return code:
< 0 = Error code
0 = No files listed
> 0 = Number of files listed
Environment
UF_UI_open_listing_window
Required License(s)
gateway
int uc4650
(
const char * dir,
int fmode,
int smode,
int * pbuf,
int * ibuf,
const char * cbuf
)
const char * | dir | Input | Input directory |
int | fmode | Input | File selection mode 1 = Select all files 2 = File template specified in cbuf 3 = Select file created/modified/ accessed after date specified in cbuf according to field specified in ibuf 4 = Select file created/modified/ accessed before date specified in cbuf according to field specified in ibuf 5 = Select file by owner specified in cbuf 6 = Select file by protection class specified in cbuf 7 = Select files of type specified in ibuf 8 = Select files by status specified in ibuf |
int | smode | Input | Sort mode 1 = Alphabetic 2 = Creation date 3 = Modified date 4 = Access date 5 = Owner |
int * | pbuf | Input | Print Field Selection Array, Set Array Element = 1 To Print Desired Field (1) = Print format (2) = Print owner (3) = Print pclass (4) = Print length (5) = Print status (6) = Print creation date (7) = Print creation time (8) = Print modification date (9) = Print modification time (10) = Print access date (11) = Print access time (12) = Print machine type (13) = Print description area (14-16) = Reserved |
int * | ibuf | Input | Integer Parameter Array IF fmode=3 or fmode=4, ibuf show date type IF ibuf(1) = 1 : use file creation date IF ibuf(1) = 2 : use file modified date IF ibuf(1) = 3 : use file accessed date IF fmode=7, ibuf selects file type set array element = 1 to select desired file type (1) = Part (2) = Symbol (3) = Text (4) = GRIP (5) = Customer (6) = UNISOLIDS (7) = UGI (8) = Communications (9) = Keystroke (10) = Display (11) = CL file (12) = Directory (13-16) = Reserved IF fmode=8, ibuf(1) = File Status |
const char * | cbuf | Input | Character Parameter IF fmode=2, cbuf contains file template IF fmode=3, cbuf contains file date IF fmode=4, cbuf contains file date IF fmode=5, cbuf contains owner name IF fmode=6, cbuf contains protection class |
uc4901 (view source)
Defined in: uf_cfi.h
Overview
Return the language name stored in the native binary file.
You can use the returned language name string
to differentiate languages that use the same character set.
NOTE: If a Native Binary File has not been loaded then uc4901
returns "ENGLISH".
Return
Return code
0 = No error
not 0 = Error code
Environment
Internal and External
Required License(s)
gateway
int uc4901
(
char lname [ MAX_FSPEC_BUFSIZE ]
)
char | lname [ MAX_FSPEC_BUFSIZE ] | Output | Returns The Language Name Stored In The Native Binary File |
UF_CFI_ask_file_exist (view source)
Defined in: uf_cfi.h
Overview
Test if a file exists.
Note: This function only works with files - not directories. To check if a
directory exists use uc4560 and pass a file type of 100.
Return
0 - No error
Otherwise - Error Code
Environment
Internal and External
History
Originally released in V16.0
Required License(s)
gateway
int UF_CFI_ask_file_exist
(
const char * file_spec,
int * status
)
const char * | file_spec | Input | The file to check |
int * | status | Output | File existence status. 0 - file exists 1 - file does not exist |
UF_CFI_spawn (view source)
Defined in: uf_cfi.h
Overview
Spawn a subprocess. The return code will indicated the status of the
process creation. If the status from the actual command is needed, use
UF_CFI_spawn_check_status.
Environment
Internal and External
See Also
UF_CFI_spawn_check_status
History
Originally released in V18.0
Required License(s)
gateway
int UF_CFI_spawn
(
const char * program,
int num_args,
char * arguments [ ] ,
logical is_concur,
int * process_id
)
const char * | program | Input | The command to be executed. This command must either be a full path name, or the program must be found on the path. |
int | num_args | Input | The number of arguments in the next array. These arguments will be passed to the command. |
char * | arguments [ ] | Input | An array of character pointers for the arguments to be passed to the program. You may pass in a NULL if there are not any arguments. These arguments will be added in the order they are stored, so the command will be: program argument[0] argument[1] ... Switches must be formatted by the caller. On NT, switches take the form "-switch:value", where on Unix switches take the form "-switch=value". |
logical | is_concur | Input | If TRUE, the command will be run at the same time as the NX Open program, if FALSE, then UF_CFI_spawn will wait for the completion of the command prior to returning to the caller. |
int * | process_id | Output | The process ID of the spawned process. This process ID can be used to check the status of the spawned process using UF_CFI_spawn_check_status. |
UF_CFI_spawn_check_status (view source)
Defined in: uf_cfi.h
Overview
Check the status of a spawned subprocess.
Environment
Internal and External
See Also
UF_CFI_spawn
History
Originally released in V18.0
Required License(s)
gateway
int UF_CFI_spawn_check_status
(
int process_id,
logical * still_running,
int * return_status
)
int | process_id | Input | The process id returned by UF_CFI_spawn for the command that was run. Note that this is only returned for processes that are run concurrently. |
logical * | still_running | Output | If TRUE, the command is still running. If FALSE, the command has completed. |
int * | return_status | Output | If still_running is FALSE, then this is the return status from the child process. If still_running is TRUE, then this will be set to zero. A return_status of 127 is set when the spawned command could not be found. |