VisualReportReportingStyleOption Enumeration¶
NXOpen.VisualReporting.VisualReport.ReportingStyleOption is an alias for NXOpen.VisualReporting.VisualReportReportingStyleOption
-
class
NXOpen.VisualReporting.
VisualReportReportingStyleOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.VisualReport.ReportingStyle
for aNXOpen.VisualReporting.VisualReport
.Enum Members
Enum Member Enum Member Description ColorObject Matching objects will be coloredTagObject Matching objects will be taggedColorAndTagObject Matching objects will be both colored and tagged-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-