VisualReportReportContextOption Enumeration¶
NXOpen.VisualReporting.VisualReport.ReportContextOption is an alias for NXOpen.VisualReporting.VisualReportReportContextOption
-
class
NXOpen.VisualReporting.
VisualReportReportContextOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.VisualReport.ReportContext
options for aNXOpen.VisualReporting.VisualReport
.Enum Members
Enum Member Enum Member Description Assembly Collect objects from entire assemblyWorkPart Collect objects from work part only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-