VisualReportExplorerReportDownStatus Enumeration¶
NXOpen.VisualReporting.VisualReportExplorer.ReportDownStatus is an alias for NXOpen.VisualReporting.VisualReportExplorerReportDownStatus
-
class
NXOpen.VisualReporting.
VisualReportExplorerReportDownStatus
¶ Bases:
object
Status reported by
NXOpen.VisualReporting.VisualReportExplorer.ReportDown
.Enum Members
Enum Member Enum Member Description None There are no objects of interest below the specified objectsEnd Report Down has reached the lowest level on all branches of the assemblyMore There are more objects of interest below the currently reported upon objects-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-