PropertyDatatypeOption Enumeration¶
NXOpen.VisualReporting.Property.DatatypeOption is an alias for NXOpen.VisualReporting.PropertyDatatypeOption
-
class
NXOpen.VisualReporting.
PropertyDatatypeOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.Property.SystemDatatype
options for a property.Enum Members
Enum Member Enum Member Description String String datatypeInteger Integer datatypeReal Floating-point datatypeBoolean Boolean datatypeUnknown The datatype is unknownNull Null data typeDate Date datatype-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-