GroupLabelDisplayStyleOption Enumeration¶
NXOpen.VisualReporting.GroupLabel.DisplayStyleOption is an alias for NXOpen.VisualReporting.GroupLabelDisplayStyleOption
-
class
NXOpen.VisualReporting.
GroupLabelDisplayStyleOption
¶ Bases:
object
Represents the possible display style options for a
NXOpen.VisualReporting.GroupLabel
.Enum Members
Enum Member Enum Member Description DeEmphasis Matching objects will be de-emphasizedSpecifiedColor Matching objects will be shown usingNXOpen.VisualReporting.GroupLabel.Color
OriginalColor Matching objects will be shown using their original colorAutomaticColor Matching objects will be shown usingNXOpen.VisualReporting.GroupLabel.Color
which is system determined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-