ClassifierRangeMethodOption Enumeration¶
NXOpen.VisualReporting.Classifier.RangeMethodOption is an alias for NXOpen.VisualReporting.ClassifierRangeMethodOption
-
class
NXOpen.VisualReporting.
ClassifierRangeMethodOption
¶ Bases:
object
Represents the possible range method options.
for a
NXOpen.VisualReporting.Classifier
.Enum Members
Enum Member Enum Member Description Number A numeric range will be usedPercentage A percentage range will be used-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-