ValidatorType Enumeration¶
-
class
NXOpen.
ValidatorType
¶ Bases:
object
validator type Enum Members
Enum Member Enum Member Description NoneValidator AnnotationValidator BaseArrowValidator BaseUserSymbolValidator CenterLineValidator CoordinateNoteValidator CurveValidator DatumTargetValidator DatumValidator DimensionValidator DrawingRegionValidator EnterpriseIdentificationValidator FCFValidator FrameBarValidator GeneralNoteValidator HatchValidator HoleTableValidator IdSymbolValidator IntersectionSymbolValidator LabelOnParentValidator Layout2dComponentValidator LocatorDesignatorValidator MaterialSpecificationValidator MemberViewValidator ModelingViewValidator ModelingViewSearchValidator NoteValidator OffsetCenterPointSymbolValidator PartIdentificationValidator PartListSectionValidator PartListValidator PMIBalloonValidator PMIPlanarCPSValidator PMILightweightSectionViewValidator PMISectionViewValidator ProcessSpecificationValidator RegionValidator SectionLineSegmentValidator SectionLineValidator SecurityMarkingValidator SpecificNoteValidator SurfaceFinishValidator TabnotSectionValidator TabnotValidator TargetPointSymbolValidator ThreadCurveValidator TitleBlockValidator VDCurveValidator ViewBreakValidator ViewingDirectionArrowValidator ViewingDirectionArrowLabelValidator ViewLabelValidator ViewValidator WeldValidator -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-