Validation Class¶
-
class
NXOpen.
Validation
¶ Bases:
NXOpen.NXObject
Represents an NX
NXOpen.Validation
object.To create a new instance of this class, use
NXOpen.ValidationCollection.Create
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Requirement | Returns or sets the requirement path. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Add | Add a objects to the validation map |
Delete | Delete Validation Object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Evaluate | Manually validate @return |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAssociatedObjects | Gets associated objects for the check. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCheckResult | The validation result. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetInitialResult | The initial result. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetKeyType | Get key type @return |
GetKeys | Get keys @return keys in the map |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetSuppressed | The suppress state of the validation @return Supress flag true = supress false unsupress |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Information | Information display on a Validation Object |
Lookup | Lookup a objects to the validation map @return objects associate with the key |
LookupInteger | Lookup a integer to the validation map |
LookupNumber | Lookup a real to the validation map |
LookupText | Lookup a text to the validation map |
LookupTime | Lookup a time to the validation map |
Prints a representation of this object to the system log file. | |
Remove | Remove a key from the map |
Replace | Replace objects of a key in the validation map |
SetAssociatedObjects | Specifies or removes associated objects for the check. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCheckResult | Set the result of validation. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSuppressed | |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUpdateControl | Define the update behavior of the validation object |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetUserClassName | Set user class name |
Enumerations¶
ValidationInputType Enumeration | Specifies the input type |
ValidationMapType Enumeration | Specifies the map types |
ValidationResult Enumeration | Specifies result of the validation |
ValidationUpdateTime Enumeration | Specifies when to validate |
Property Detail¶
IsOccurrence¶
-
Validation.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Validation.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Validation.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Validation.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Validation.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Validation.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Requirement¶
-
Validation.
Requirement
¶ Returns or sets the requirement path.
-------------------------------------
Getter Method
Signature
Requirement()
Returns: requirement path Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Requirement(requirement)
Parameters: requirement (str) – requirement path New in version NX8.0.0.
License requirements: None.
Method Detail¶
Add¶
-
Validation.
Add
¶ Overloaded method Add
Add(key, objs)
Add(key, text)
Add(key, number)
Add(key, number)
Add(key, day, time)
-------------------------------------
Add a objects to the validation map
Signature
Add(key, objs)
Parameters: - key (str) – Map key
- objs (list of
NXOpen.NXObject
) – Objects to be associate with the key
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Add a text to the validation map
Signature
Add(key, text)
Parameters: - key (str) – Map key
- text (str) – Text to be associate with the key
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Add a real to the validation map
Signature
Add(key, number)
Parameters: - key (str) – Map key
- number (float) – Real to be associate with the key
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Add a integer to the validation map
Signature
Add(key, number)
Parameters: - key (str) – Map key
- number (int) – Integer to be associate with the key
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Add a time to the validation map
Signature
Add(key, day, time)
Parameters: - key (str) – Map key
- day (int) – Date to be associated with the key
- time (int) – Time to be associate with the key
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Delete¶
-
Validation.
Delete
¶ Delete Validation Object
Signature
Delete()
New in version NX4.0.0.
License requirements: None.
Evaluate¶
-
Validation.
Evaluate
¶ Manually validate
Signature
Evaluate()
Returns: Return type: NXOpen.ValidationResult
New in version NX4.0.0.
License requirements: None.
FindObject¶
-
Validation.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAssociatedObjects¶
-
Validation.
GetAssociatedObjects
¶ Gets associated objects for the check.
Signature
GetAssociatedObjects()
Returns: Objects associated with the check Return type: list of NXOpen.NXObject
New in version NX8.5.0.
License requirements: None.
GetCheckResult¶
-
Validation.
GetCheckResult
¶ The validation result.
Result is represented as a Name, with the following options: pass : Validation Pass all checks information : Validation Pass with information warning : Validation Pass with warning failed : Validation Failed unknown : Unknown validation result
Signature
GetCheckResult()
Returns: Return type: NXOpen.ValidationResult
New in version NX4.0.0.
License requirements: None.
GetInitialResult¶
-
Validation.
GetInitialResult
¶ The initial result.
Signature
GetInitialResult()
Returns: result of validation object. Return type: NXOpen.ValidationResult
New in version NX4.0.0.
License requirements: None.
GetKeyType¶
-
Validation.
GetKeyType
¶ Get key type
Signature
GetKeyType(key)
Parameters: key (str) – Map key Returns: Return type: NXOpen.ValidationMapType
New in version NX4.0.0.
License requirements: None.
GetKeys¶
-
Validation.
GetKeys
¶ Get keys
Signature
GetKeys()
Returns: keys in the map Return type: list of str New in version NX4.0.0.
License requirements: None.
GetSuppressed¶
-
Validation.
GetSuppressed
¶ The suppress state of the validation
Signature
GetSuppressed()
Returns: Supress flag true = supress false unsupress Return type: bool New in version NX4.0.0.
License requirements: None.
Information¶
-
Validation.
Information
¶ Information display on a Validation Object
Signature
Information()
New in version NX4.0.0.
License requirements: None.
Lookup¶
-
Validation.
Lookup
¶ Lookup a objects to the validation map
Signature
Lookup(key)
Parameters: key (str) – Map key Returns: objects associate with the key Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: None.
LookupInteger¶
-
Validation.
LookupInteger
¶ Lookup a integer to the validation map
Signature
LookupInteger(key)
Parameters: key (str) – Map key Returns: a tuple Return type: A tuple consisting of (number, found). number is a int. Integer associate with the key found is a bool. True integer found False not found in map New in version NX4.0.0.
License requirements: None.
LookupNumber¶
-
Validation.
LookupNumber
¶ Lookup a real to the validation map
Signature
LookupNumber(key)
Parameters: key (str) – Map key Returns: a tuple Return type: A tuple consisting of (number, found). number is a float. Number associate with the key found is a bool. True text found False not found in map New in version NX4.0.0.
License requirements: None.
LookupText¶
-
Validation.
LookupText
¶ Lookup a text to the validation map
Signature
LookupText(key)
Parameters: key (str) – Map key Returns: a tuple Return type: A tuple consisting of (text, found). text is a str. Text associate with the key found is a bool. True text found False not found in map New in version NX4.0.0.
License requirements: None.
LookupTime¶
-
Validation.
LookupTime
¶ Lookup a time to the validation map
Signature
LookupTime(key)
Parameters: key (str) – Map key Returns: a tuple Return type: A tuple consisting of (day, time, found). day is a int. Date associate with the key time is a int. Time associate with the key found is a bool. True time found False not found in map New in version NX4.0.0.
License requirements: None.
Print¶
-
Validation.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Remove¶
-
Validation.
Remove
¶ Remove a key from the map
Signature
Remove(key)
Parameters: key (str) – Map key New in version NX4.0.0.
License requirements: None.
Replace¶
-
Validation.
Replace
¶ Replace objects of a key in the validation map
Signature
Replace(key, objs)
Parameters: - key (str) – Map key
- objs (list of
NXOpen.NXObject
) – Objects to be associate with the key
New in version NX4.0.0.
License requirements: None.
SetAssociatedObjects¶
-
Validation.
SetAssociatedObjects
¶ Specifies or removes associated objects for the check.
Signature
SetAssociatedObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) – Objects to be associated with the checkNew in version NX8.5.0.
License requirements: None.
SetCheckResult¶
-
Validation.
SetCheckResult
¶ Set the result of validation.
Result is represented as a Name, with the following options: pass : Validation Pass all checks information : Validation Pass with information warning : Validation Pass with warning failed : Validation Failed unknown : Unknown validation result
Signature
SetCheckResult(result)
Parameters: result ( NXOpen.ValidationResult
) –New in version NX4.0.0.
License requirements: None.
SetName¶
-
Validation.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSuppressed¶
-
Validation.
SetSuppressed
¶ Signature
SetSuppressed(suppress)
Parameters: suppress (bool) – Suppress flag true = supress, false = unsupress New in version NX4.0.0.
License requirements: None.
SetUpdateControl¶
-
Validation.
SetUpdateControl
¶ Define the update behavior of the validation object
Signature
SetUpdateControl(updateTime)
Parameters: updateTime ( NXOpen.ValidationUpdateTime
) – Sets the time of updateNew in version NX4.0.0.
License requirements: None.