RequirementCollection Class¶
-
class
NXOpen.Validate.
RequirementCollection
¶ Bases:
object
Represents an NX
NXOpen.Validate.RequirementCollection
object.To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
RevisionRule | Returns or sets the revision rule for requirement from Teamcenter |
Methods¶
Method | Description |
---|---|
CreateRequirementBuilder | Creates a NXOpen.Validate.RequirementBuilder @return |
FindObject | Finds the NXOpen.Validate.Requirement with the given identifier. |
LoadFromExternalSource | Loads NXOpen.Validate.Requirement from external source. |
RefreshFromExternalSource | Refreshes the requirements from external source. |
Enumerations¶
RequirementCollectionSourceTypeOptions Enumeration | This enum represents the type of external source where requirement is defined |
Property Detail¶
RevisionRule¶
-
RequirementCollection.
RevisionRule
¶ Returns or sets the revision rule for requirement from Teamcenter
-------------------------------------
Getter Method
Signature
RevisionRule()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevisionRule(rule)
Parameters: rule (str) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
CreateRequirementBuilder¶
-
RequirementCollection.
CreateRequirementBuilder
¶ Creates a
NXOpen.Validate.RequirementBuilder
Signature
CreateRequirementBuilder(requirement)
Parameters: requirement ( NXOpen.Validate.Requirement
) –Returns: Return type: NXOpen.Validate.RequirementBuilder
New in version NX8.5.0.
License requirements: None.
FindObject¶
-
RequirementCollection.
FindObject
¶ Finds the
NXOpen.Validate.Requirement
with the given identifier.An exception will be thrown if no object can be found with given identifier.
Signature
FindObject(id)
Parameters: id (str) – The identifier of the NXOpen.Validate.Requirement
Returns: NXOpen.Validate.Requirement
with the identifierReturn type: NXOpen.Validate.Requirement
New in version NX8.5.0.
License requirements: None.
LoadFromExternalSource¶
-
RequirementCollection.
LoadFromExternalSource
¶ Loads
NXOpen.Validate.Requirement
from external source.The source can be local file, Teamcenter requirement item or item revision, and Teamcenter spreadsheet dataset for which the input sourceType is LocalFile, Teamcenter and TeamcenterFile respectively. <br/> Example inputs when sourceType is LocalFile
- source: “C:requirement.xml” or “C:requirement_spreadsheet.xls”
- revision: empty string
- project: “category_A” It’s a project node name in the source XML file or a sheet name in the source spreadsheet file.
<br/> Example inputs when sourceType is Teamcenter
- If source is item revision 000084/A:
- source: “000084”
- revision: “A”
- project: empty string
- If source is item 000084:
- source: “000084”
- revision:empty string
- project: empty string
<br/> Example inputs when sourceType is TeamcenterFile
- If source is a spreadsheet dataset in an item revision 000085/A:
- source: 000085
- revision: A
- project: “category_A” It’s a sheet name in the source spreadsheet.
- If source is a spreadsheet dataset in item 000085:
- source: “000085”
- revision: empty string
- project: “category_A” It’s a sheet name in the source spreadsheet.
Signature
LoadFromExternalSource(sourceType, source, revision, project)
Parameters: - sourceType (
NXOpen.Validate.RequirementCollectionSourceTypeOptions
) – Type of the external source - source (str) – File full path if sourceType is LocalFile; Item id if sourceType is Teamcenter or TeamcenterFile.
- revision (str) – Only needed if sourceType is Teamcenter or TeamcenterFile. Revision id if source is an item revision. Null if source is an item.
- project (str) – Required if sourceType is LocalFile or TeamcenterFile. Project name if the source is a XML file; Sheet name if source is a spreadsheet file.
New in version NX8.5.0.
License requirements: None.
RefreshFromExternalSource¶
-
RequirementCollection.
RefreshFromExternalSource
¶ Refreshes the requirements from external source.
Signature
RefreshFromExternalSource(requirementTags)
Parameters: requirementTags (list of NXOpen.Validate.Requirement
) –New in version NX10.0.0.
License requirements: None.