ParserDataSourceTypes Enumeration¶
NXOpen.Validate.Parser.DataSourceTypes is an alias for NXOpen.Validate.ParserDataSourceTypes
-
class
NXOpen.Validate.
ParserDataSourceTypes
¶ Bases:
object
The data source type of check result.
Enum Members
Enum Member Enum Member Description MostRecentRun Result of most recent runResultFromPart Result from partResultFromTeamcenter Result from TeamcenterResultFromNXChecks Result from NX checksResultFromLogFile Result from Log File-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-