VRMLImporter Class¶
-
class
NXOpen.
VRMLImporter
¶ Bases:
NXOpen.Importer
Used to import a VRML file into the work part.
To obtain an instance of this class use
ImportManager.CreateVrmlImporter
.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AllLevelsOfDetail | Returns or sets the All Levels of Detail flag. |
AngularTolerance | Returns or sets the angular tolerance. |
FileName | Returns or sets the name of the file containing the data to import. |
FileUnits | Returns or sets the file units. |
GenerateOneModel | Returns or sets the Generate One Model flag. |
HideSmoothEdges | Returns or sets the Hide Smooth Edges flag. |
MoreSummaryDetails | Returns or sets the More Summary Details flag. |
SuppressWarningMessages | Returns or sets the Suppress Warning Messages flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VRMLImporterAngularToleranceType Enumeration | Specifies the angular tolerance. |
VRMLImporterFileUnitsType Enumeration | Specifies the VRML file units. |
Property Detail¶
AllLevelsOfDetail¶
-
VRMLImporter.
AllLevelsOfDetail
¶ Returns or sets the All Levels of Detail flag.
True if the All Levels of Detail flag is on.
-------------------------------------
Getter Method
Signature
AllLevelsOfDetail()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllLevelsOfDetail(allLevelsOfDetail)
Parameters: allLevelsOfDetail (bool) – New in version NX5.0.0.
License requirements: None.
AngularTolerance¶
-
VRMLImporter.
AngularTolerance
¶ Returns or sets the angular tolerance.
-------------------------------------
Getter Method
Signature
AngularTolerance()
Returns: Return type: NXOpen.VRMLImporterAngularToleranceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance(angularTolerance)
Parameters: angularTolerance ( NXOpen.VRMLImporterAngularToleranceType
) –New in version NX5.0.0.
License requirements: None.
FileUnits¶
-
VRMLImporter.
FileUnits
¶ Returns or sets the file units.
-------------------------------------
Getter Method
Signature
FileUnits()
Returns: Return type: NXOpen.VRMLImporterFileUnitsType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileUnits(fileUnits)
Parameters: fileUnits ( NXOpen.VRMLImporterFileUnitsType
) –New in version NX5.0.0.
License requirements: None.
GenerateOneModel¶
-
VRMLImporter.
GenerateOneModel
¶ Returns or sets the Generate One Model flag.
True if the Generate One Model flag is on.
-------------------------------------
Getter Method
Signature
GenerateOneModel()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerateOneModel(generateOneModel)
Parameters: generateOneModel (bool) – New in version NX5.0.0.
License requirements: None.
HideSmoothEdges¶
-
VRMLImporter.
HideSmoothEdges
¶ Returns or sets the Hide Smooth Edges flag.
True if the Hide Smooth Edges flag is on.
-------------------------------------
Getter Method
Signature
HideSmoothEdges()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HideSmoothEdges(hideSmoothEdges)
Parameters: hideSmoothEdges (bool) – New in version NX5.0.0.
License requirements: None.
MoreSummaryDetails¶
-
VRMLImporter.
MoreSummaryDetails
¶ Returns or sets the More Summary Details flag.
True if the More Summary Details flag is on.
-------------------------------------
Getter Method
Signature
MoreSummaryDetails()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoreSummaryDetails(moreSummaryDetails)
Parameters: moreSummaryDetails (bool) – New in version NX5.0.0.
License requirements: None.
SuppressWarningMessages¶
-
VRMLImporter.
SuppressWarningMessages
¶ Returns or sets the Suppress Warning Messages flag.
True if the Suppress Warning Messages flag is on.
-------------------------------------
Getter Method
Signature
SuppressWarningMessages()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuppressWarningMessages(suppressWarningMessages)
Parameters: suppressWarningMessages (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
VRMLImporter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.