UnitCollection Class¶
-
class
NXOpen.
UnitCollection
¶ Bases:
object
Provides methods for manipulating the units in a part
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Convert | Convert a value from one unit of measure to another @return |
FindObject | Finds the Unit with the given identifier as recorded in a journal. |
GetBase | Find the base part unit for a given type of measure @return base unit |
GetMeasureTypes | Finds the units that are available for a given type of measure @return Array of units for a given measurement type |
GetMeasures | Finds the list of different types of measures available in the system. |
Method Detail¶
Convert¶
-
UnitCollection.
Convert
¶ Convert a value from one unit of measure to another
Signature
Convert(initialUnit, targetUnit, initialValue)
Parameters: - initialUnit (
NXOpen.Unit
) – initial measurement unit - targetUnit (
NXOpen.Unit
) – target measurement unit - initialValue (float) –
Returns: Return type: float
New in version NX4.0.0.
License requirements: None.
- initialUnit (
FindObject¶
-
UnitCollection.
FindObject
¶ Finds the
Unit
with the given identifier as recorded in a journal. An exception will be thrown if no object can be found with the given journal identifier.Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Unit found Return type: NXOpen.Unit
New in version NX4.0.0.
License requirements: None.
GetBase¶
-
UnitCollection.
GetBase
¶ Find the base part unit for a given type of measure
Signature
GetBase(measureName)
Parameters: measureName (str) – the type of measure NOTE: The full Unicode character set is not supported for this parameter. Returns: base unit Return type: NXOpen.Unit
New in version NX4.0.0.
License requirements: None.
GetMeasureTypes¶
-
UnitCollection.
GetMeasureTypes
¶ Finds the units that are available for a given type of measure
Signature
GetMeasureTypes(measureName)
Parameters: measureName (str) – the type of measure NOTE: The full Unicode character set is not supported for this parameter. Returns: Array of units for a given measurement type Return type: list of NXOpen.Unit
New in version NX4.0.0.
License requirements: None.
GetMeasures¶
-
UnitCollection.
GetMeasures
¶ Finds the list of different types of measures available in the system.
Types of measures include length, area and volume
Signature
GetMeasures()
Returns: Array of names of measure types Return type: list of str New in version NX4.0.0.
License requirements: None.