Styler Class¶
Methods¶
Method | Description |
---|---|
CreateStylerDialog | Creates an NX (UIStyler generated) bottom dialog. |
Method Detail¶
CreateStylerDialog¶
-
Styler.
CreateStylerDialog
¶ Creates an NX (UIStyler generated) “bottom” dialog.
The ”.dlg” file can only be generated from the Open UIStyler.
Signature
CreateStylerDialog(dialogName)
Parameters: dialogName (str) – Dialog name NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: NXOpen.UIStyler.Dialog
New in version NX5.0.0.
License requirements: None.