RealScale Class¶
-
class
NXOpen.UIStyler.
RealScale
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a RealScale for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the item value |
Sensitivity | Returns or sets the sensitivity |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddDragHandler | Registers dtag callback. |
AddValueChangedHandler | Called when a dialog user moves the slider up and down the scale. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetDecimalPrecision | Sets decimal precision |
SetLabels | Sets labels |
SetLimits | Sets limits |
Property Detail¶
ItemValue¶
-
RealScale.
ItemValue
¶ Returns or sets the item value
-------------------------------------
Getter Method
Signature
ItemValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue(itemVal)
Parameters: itemVal (float) – New real value for the slider. It must be within the min/max range New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
RealScale.
Sensitivity
¶ Returns or sets the sensitivity
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – TRUE if sensitive, FALSE if insensitive New in version NX5.0.0.
License requirements: None.
Visibility¶
-
RealScale.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddDragHandler¶
-
RealScale.
AddDragHandler
¶ Registers dtag callback.
This method should be called before calling
UIStyler.Dialog.Show
orUIStyler.Dialog.RegisterWithUiMenu
Signature
AddDragHandler(dragevent, isDialogLaunchingEvent)
Parameters: - dragevent (CallableObject) – Callback for add drag event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
AddValueChangedHandler¶
-
RealScale.
AddValueChangedHandler
¶ Called when a dialog user moves the slider up and down the scale.
For example, if a user moves the slider from 0.0 to 10.0, the dialog calls the drag callback 100 times, one for each value that the slider moves across. Do not terminate the dialog with a drag callback. The dialog should always return UF_UI_CB_CONTINUE_DIALOG.
Signature
AddValueChangedHandler(valuechangedevent, isDialogLaunchingEvent)
Parameters: - valuechangedevent (CallableObject) – Callback for value changed event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
SetDecimalPrecision¶
-
RealScale.
SetDecimalPrecision
¶ Sets decimal precision
Signature
SetDecimalPrecision(digits)
Parameters: digits (int) – The number significant digits New in version NX5.0.0.
License requirements: None.
SetLabels¶
-
RealScale.
SetLabels
¶ Sets labels
Signature
SetLabels(minimumLabel, maximumLabel)
Parameters: - minimumLabel (str) – String minimum label NOTE: The full Unicode character set is not supported for this parameter.
- maximumLabel (str) – String maximum label NOTE: The full Unicode character set is not supported for this parameter.
New in version NX5.0.0.
License requirements: None.