FileOperationDataFileOperationType Enumeration¶
NXOpen.UIStyler.FileOperationData.FileOperationType is an alias for NXOpen.UIStyler.FileOperationDataFileOperationType
-
class
NXOpen.UIStyler.
FileOperationDataFileOperationType
¶ Bases:
object
Describes file operation
Enum Members
Enum Member Enum Member Description New New file operationOpen Open file operationSave Save file operationSaveAs Save as file operationSaveAll Save all file operationClose Close file operationQuit Quit file operationSaveAndExit Save and Exit file operationChangePart Chaneg part file operationExecute Execute file operationReopen Reopen file operationSaveAllAndClose Save all and close file operationSaveAndClose Save and close file operationSaveAsAndClose Save as and close file operation-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-