FileOperationDataFileOperationState Enumeration¶
NXOpen.UIStyler.FileOperationData.FileOperationState is an alias for NXOpen.UIStyler.FileOperationDataFileOperationState
-
class
NXOpen.UIStyler.
FileOperationDataFileOperationState
¶ Bases:
object
Describes file state
Enum Members
Enum Member Enum Member Description Enter Enter file stateExit Exit file state-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-