CollapsibleGroup Class

class NXOpen.UIStyler.CollapsibleGroup

Bases: NXOpen.UIStyler.StylerItem

Represents a Collapsible Group for UI Styler

New in version NX5.0.0.

Properties

Property Description
CollapseState Returns or sets the collapse-state
Visibility Returns or sets the visibility

Methods

Method Description
Dispose Free resources associated with the instance.
GetItemType Gets the dialog item type.
InitializeAttachment Returns initialized dialog item attachment information @return attachment object
IsEqualTo Equates two styler items @return
SetAttachment Specifies the updated dialog item attachment information
SetLabel Sets label of collapsible group

Property Detail

CollapseState

CollapsibleGroup.CollapseState

Returns or sets the collapse-state

-------------------------------------

Getter Method

Signature CollapseState()

Returns:
Return type:bool

New in version NX6.0.5.

License requirements: None.

-------------------------------------

Setter Method

Signature CollapseState(itemVal)

Parameters:itemVal (bool) –

New in version NX6.0.5.

License requirements: None.

Visibility

CollapsibleGroup.Visibility

Returns or sets the visibility

-------------------------------------

Getter Method

Signature Visibility()

Returns:
Return type:bool

New in version NX6.0.5.

License requirements: None.

-------------------------------------

Setter Method

Signature Visibility(type)

Parameters:type (bool) –

New in version NX6.0.5.

License requirements: None.

Method Detail

SetLabel

CollapsibleGroup.SetLabel

Sets label of collapsible group

Signature SetLabel(strLabel)

Parameters:strLabel (str) – Text to be set as label NOTE: The full Unicode character set is not supported for this parameter.

New in version NX6.0.5.

License requirements: None.