BitMap Class¶
-
class
NXOpen.UIStyler.
BitMap
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Bit Map for UI Styler.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetBitmap | Sets the bitmap filename. |
Method Detail¶
SetBitmap¶
-
BitMap.
SetBitmap
¶ Sets the bitmap filename.
The filename extension must be: .UBM, .XPM, or .BMP. The bitmap can be of any size.
Signature
SetBitmap(bitmap)
Parameters: bitmap (str) – filename with .ubm, .xpm, or .bmp extension that contains bitmap definition NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.