Attachment Class¶
-
class
NXOpen.UIStyler.
Attachment
¶ Bases:
NXOpen.TransientObject
Represents an Attachment for UI Styler
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
SetAttachTypeLeft | Sets the attach type left |
SetAttachTypeRight | Sets the attach type right |
SetAttachTypeTop | Sets the attach type top |
SetCenter | Sets whether the dialog item is at the center |
SetLeftDialogItem | Sets the left dialog item |
SetLeftOffset | Sets the left offset |
SetRightDialogItem | Sets the right dialog item |
SetRightOffset | Sets the right offset |
SetTopDialogItem | Sets the top dialog item |
SetTopOffset | Sets the top offset |
Enumerations¶
AttachmentAttachType Enumeration | Represents alignment option for Styler Item |
Method Detail¶
Dispose¶
-
Attachment.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET or Java, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
SetAttachTypeLeft¶
-
Attachment.
SetAttachTypeLeft
¶ Sets the attach type left
Signature
SetAttachTypeLeft(attachTypeLeft)
Parameters: attachTypeLeft ( NXOpen.UIStyler.AttachmentAttachType
) –New in version NX5.0.0.
License requirements: None.
SetAttachTypeRight¶
-
Attachment.
SetAttachTypeRight
¶ Sets the attach type right
Signature
SetAttachTypeRight(attachTypeRight)
Parameters: attachTypeRight ( NXOpen.UIStyler.AttachmentAttachType
) –New in version NX5.0.0.
License requirements: None.
SetAttachTypeTop¶
-
Attachment.
SetAttachTypeTop
¶ Sets the attach type top
Signature
SetAttachTypeTop(attachTypeTop)
Parameters: attachTypeTop ( NXOpen.UIStyler.AttachmentAttachType
) – attach_type_topNew in version NX5.0.0.
License requirements: None.
SetCenter¶
-
Attachment.
SetCenter
¶ Sets whether the dialog item is at the center
Signature
SetCenter(isCenter)
Parameters: isCenter (bool) – center New in version NX5.0.0.
License requirements: None.
SetLeftDialogItem¶
-
Attachment.
SetLeftDialogItem
¶ Sets the left dialog item
Signature
SetLeftDialogItem(leftItemIdentifire)
Parameters: leftItemIdentifire (str) – Left item identifier NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.
SetLeftOffset¶
-
Attachment.
SetLeftOffset
¶ Sets the left offset
Signature
SetLeftOffset(offsetLeft)
Parameters: offsetLeft (int) – New in version NX5.0.0.
License requirements: None.
SetRightDialogItem¶
-
Attachment.
SetRightDialogItem
¶ Sets the right dialog item
Signature
SetRightDialogItem(rightItemIdentifire)
Parameters: rightItemIdentifire (str) – Right item identifier NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.
SetRightOffset¶
-
Attachment.
SetRightOffset
¶ Sets the right offset
Signature
SetRightOffset(offsetRight)
Parameters: offsetRight (int) – New in version NX5.0.0.
License requirements: None.
SetTopDialogItem¶
-
Attachment.
SetTopDialogItem
¶ Sets the top dialog item
Signature
SetTopDialogItem(topItemIdentifire)
Parameters: topItemIdentifire (str) – Top item identifier NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.