NXOpen.UF.Trns.CreateRotationMatrix

Trns.CreateRotationMatrix()

Refer to UF_TRNS_create_rotation_matrix for documentation.

Signature: CreateRotationMatrix(origin, direction, degreesRotation)

Parameters:
  • origin (list of float) – Origin Of The Axis - Absolute Coordinates
  • direction (list of float) – Direction Vector - Absolute Coordinates
  • degreesRotation (float) – Rotation Angle In Degrees
Returns:

A Tuple

Return type:

A tuple consisting of (matrix,status)

matrix(list of float): Rotation Matrix. This must be declared to hold 12 doubles.

status(int): Status Code 0 - Success 1 - Direction Vector Is A Zero Vector

License requirements: None