NXOpen.UF.ModlGeneral.CreateBsurfThruPts¶
-
ModlGeneral.
CreateBsurfThruPts
()¶ Refer to UF_MODL_create_bsurf_thru_pts for documentation.
Signature:
CreateBsurfThruPts(createMode, uClosedStatus, vClosedStatus, uDegree, vDegree, numRows, ptsInfoPerRow)
Parameters: - createMode (int) – Creation mode = 1 -> specified points should lie on the B-surface = 2 -> specified points should be used as the con trol vertices = 3 -> specified points should be used as the control vertices along with using the specified weight information
- uClosedStatus (int) – Open/closed status in u direction = 0 -> open = 1 -> closed
- vClosedStatus (int) – Open/closed status in v direction = 0 -> open = 1 -> closed
- uDegree (int) – Degree in u direction
- vDegree (int) – Degree in v direction
- numRows (int) – Number of rows of points
- ptsInfoPerRow (list of
NXOpen.UF.Modl.BsurfRowInfo
Refer to UF_MODL_bsurf_row_info_s for documentation.) – Points information for each row. This is an array of UF_MODL_bsurf_row_info_t structures dimensioned to num_rows.
Returns: Tag of the created B-surface
Return type: Tag
License requirements: SOLIDS MODELING and FREE-FORM MODELING or Basic Freeform Modeling