NXOpen.UF.Modeling.Compare¶
-
Modeling.
Compare
()¶ Refer to UF_MODL_compare for documentation.
Signature:
Compare(object1, object2, relation)
Parameters: - object1 (Tag) – Object identifier of first object (valid objects are faces and edges)
- object2 (Tag) – Object identifier of second object (valid objects are faces and edges)
- relation (int) – Relation to be used for comparison. 1 = Geometric Equivalence
Returns: 1 = If the relation exists between two objects 0 = Otherwise
Return type: int
License requirements: SOLIDS MODELING