NXOpen.UF.Mfm.CreateMachiningFeaturesFromModelingFeatures¶
-
Mfm.
CreateMachiningFeaturesFromModelingFeatures
()¶ Refer to UF_MFM_create_machining_features_from_modeling_features for documentation.
Signature:
CreateMachiningFeaturesFromModelingFeatures(bodyCount, bodyList, typeCount, featureTypes)
Parameters: - bodyCount (int) – The number of bodies
- bodyList (list of Tag) – The list of bodies
- typeCount (int) – The number of feature types
- featureTypes (list of str) – The list of feature type names
Returns: A Tuple
Return type: A tuple consisting of (count,machining_features)
count(int): The of machining feature
machining_features(list of PointerWrapper): The array of machining fetures The memory is allocated by this function and must be freed by calling UF_free.
License requirements: None